STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1637 Views
  • 0 replies
  • 2 kudos

BUG: STM32CubeIDE 1.6.1 code generator fails to generate SysTick_Handler () if used with RTOS and non-systick timer as timebase source

Using STM32CubeIDE 1.6.1 with a project based on Version 1.6.0 of the STM32H7 firmware package the code generator will not generate a void SysTick_Handler (void) { method as long as according to the recommendation a non-systick-timer is configured as...

MNagl.1 by Associate II
  • 829 Views
  • 0 replies
  • 0 kudos

Resolved! usb high speed phy not work

mcu: STM32H743IITxhardware: USB_HS1 + usb3300 physoftware: usb host mode with all classesAll code are generated by cubemx 6.1.1, and I trace the usb data on wire with usb data analyzer.if OTG's internal DMA disabled, full speed usb device works ok, b...

shark by Senior
  • 3276 Views
  • 5 replies
  • 0 kudos

Resolved! Does DFSDM limit SYSCLK frequency? (the problem)

I am trying to set up DFSDM clock for STM32H7A3VITx and external 10MHz Manchester-encoding modulator using CubeMX.Since Manchester requires DFSDM clock at least 6x higher than modulator clock, minimum clock frequency is 60MHz.The only two *active* cl...

0693W000008yKWdQAM.png
TDJ by Lead
  • 2513 Views
  • 4 replies
  • 0 kudos

Resolved! How to set up DFSDM with timer in CubeMX?

In CubeMX I am trying to put together DFSDM setup described in STM32L4 workshop: 4.6 New peripherals - DFSDM - App example 2 (PT100 thermometer) but for STM32H7A3VITx. Objective: fill the filter buffer with N samples every 1s. Screenshots below.I got...

0693W000008yYmGQAU.png 0693W000008yYmLQAU.png 0693W000008yaaRQAQ.png
TDJ by Lead
  • 1590 Views
  • 1 replies
  • 0 kudos

IDE version update , compat table with MX parts CHAOS

Some months i use check update in my testing IDE 1.5.1 instalation and it reports NO UPDATE. Now in software packages arrive TouchGFX 16.1 and is marked as not compatible with IDE. Why this simple think dont work? Next part is internal IDE MX plugin ...

MM..1 by Chief III
  • 958 Views
  • 1 replies
  • 1 kudos