STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Resolved! ADC DMA_Handle is 0!

HiI'm using a NUCLEO-H7A3ZI-Q.I have created a project with CubeMX and I'm experiencing a strange behaviour on the ADC.The initialisation code is calling  MX_ADC1_Init() but this function returns with an error but the ADC DMA_Handle is 0, causing lat...

EGonc.3 by Associate II
  • 2439 Views
  • 3 replies
  • 0 kudos

Resolved! CubeIDE 1.7.0 programming Nucleo-H723ZG to respond to UART input using DMA receive. Code generated by MX results in received data ec as all zeros. Is this a known MX-generated code error?

The MX generated C code issues the USART initiation call before the DMA initiation call. My code simply echoes back any text received by the USART. Unfortunately the echoed data (correct length) is all zeros. The UART read buffer is initialised with ...

MKidd.1 by Associate II
  • 7115 Views
  • 16 replies
  • 0 kudos

STM32H747XI Timer Input Capture Not Working

Hello,I'm trying to use a timer to measure the frequency of an input signal using the callback function:HAL_TIM_IC_CaptureCallBack(TIM_HandleTypeDef*htim)The function never seems to be called when a voltage is applied to the input pin. Here is the ti...

AWats.4 by Associate II
  • 2762 Views
  • 3 replies
  • 0 kudos

Possible CubeMX I2C timing config bug (STM32L0x and other)

I try to complete standard I2C 100kHz setup for STM32L041 with 16MHz clock (I2C1CLK). Here are CubeMX setting:Timing registry value is 0x00A03D53 which, according to RM0377, 23.7.5 Timing register (I2C_TIMINGR), translates to:PRESC=0SCLDEL=10SDADEL=0...

0693W00000Dq1KcQAJ.png 0693W00000Dq1LpQAJ.png
TDJ by Lead
  • 2073 Views
  • 2 replies
  • 0 kudos

Invalid usbd_conf.c generated by STM32Cube v6.3.0

Output in the usbd_conf.c file when generating code for a CDC device. Code is using USE_HAL_PCD_REGISTER_CALLBACK for HAL_PCD_MspInit and HAL_PCD_MspDeInit instead of USE_HAL_PCD_REGISTER_CALLBACKS (note the final 'S'), which was there in previous ve...

0693W00000DqNvGQAV.png
pbk by Associate
  • 2009 Views
  • 4 replies
  • 0 kudos

Is it possible to use the internal OPAMP from the STM32G4 series with only the VINPx pin assigned to a physical pin? Configured as non-inverting, negative feedback with a gain.

I would like to implement a current sensing using a grounded shunt resistor. Therefore I would like to use the build-in OPAMP from the STM32G491 Series. But I'm not satisfied with the CubeMX configuration.In AN5306 I found a configuration under 4.4.1...

MWält.2 by Associate II
  • 2351 Views
  • 3 replies
  • 1 kudos

Resolved! How do I report an error in Cube initialization code?

I am using stm32L412CBU microcontroller and I am using both ADC units. The code generation generates this line of code:PeriphClkInit.AdcClockSelection = ADCCLockSelection; which is incorrect according to the structure RCC_PeriphCLKInitTypeDef for th...

MKass.1 by Associate II
  • 1711 Views
  • 2 replies
  • 0 kudos