STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1626 Views
  • 0 replies
  • 2 kudos

STM32CubeMx much not edititable gray field

what happened last time (2 years.-) ? why can't I change a lot of things ?I am working on CubeMx for STM32H745ZITx ...I have loaded default project for Nucleo-144 STM32H745ZITx, and want to customise for me unfortunately many options are grey ... are...

maniek by Associate III
  • 2913 Views
  • 5 replies
  • 1 kudos

Resolved! Wrong default linker FLASH STM32L412

Hi,I think I may have found an error.When generating a project for STM32L412K8TX (not a board) the default linker file define a RAM LENGTH of 40K.The STM32L412K8TX have 40K divided in two parts, 32K in RAM1 (0x20000000) and 8K in RAM2 (0x10000000).Pa...

svalsesia by Associate II
  • 1478 Views
  • 2 replies
  • 0 kudos

STM32WB5MMG with ST25DV04 NFC

We want to use the X-cube-NFC4 3.0.0 library for programming the STM32WB5MMG with the ST25DV04 NFC tag. We included:Board Part NFC (NFC4 / ST25DV)Wireless lib_nfc with core and Interface (Template)Board Support STM32Cube_Custom_BSP_Drivers (Custom / ...

SimoE by Associate II
  • 1698 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeMX bug for FDCAN?

Hi STI am using STM32CubeMX v6.10.0 with selected MCU STM32H563ZITx.When configuring FDCAN1 I may have found a bug in the tool. The below two Nominal Time Seg1 and Seg2 say that the lowest value is "2" and the tool is limiting setting it to "1" which...

Imre_0-1707302997348.png Imre_1-1707303014423.png Imre_2-1707303308710.png
Imre by Associate III
  • 2515 Views
  • 3 replies
  • 1 kudos

Resolved! Controlling Servo motors with Timers problem

I set the parameter of TIM5 of my MCU on CubeMX,the frequency of the clock is 72 MHz,PSC is 7199,ARR is 199,the information about my settings is below: TIM5 is used to output 4  channels of PWM to control four SG90 servos,TIM1 toTIM4 is used to contr...

屏幕截图 2024-03-21 183646.png 屏幕截图 2024-03-21 183735.png 屏幕截图 2024-03-21 184516.png
WINNER by Associate II
  • 8280 Views
  • 4 replies
  • 1 kudos