STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

Resolved! STM32F103 & SDIO - card won't respond

Posted on February 09, 2017 at 02:08I've got a custom board with a STM32F103 that connects to a micro SD card using 1 bit SDIO. I've generated some basic test code using STM32CubeMx Rev 4.19.0 and STM32CubeF1 release 1.4.0 (both the latest according...

peterm by Associate II
  • 4057 Views
  • 5 replies
  • 0 kudos

multi ADC by IT

Hi I'm using 2ch in ADC1 of STM32H735VGT.I set PIN15 to timer 5 and the waveform appears weird.  What's the problem? My ADC1_Init :static void MX_ADC1_Init(void){/* USER CODE BEGIN ADC1_Init 0 *//* USER CODE END ADC1_Init 0 */ADC_MultiModeTypeDef mul...

giwonKIM by Associate III
  • 1530 Views
  • 1 replies
  • 0 kudos

Delay to Multi ADCs

 HI. I'm using 3ch in ADC3 of STM32H735VGT. They are running in Continuous conversion mode without delay. Do I have to give a delay after one conversion? If so, how long should I delay? Thank you.  static void MX_ADC1_Init(void){/* USER CODE BEGIN AD...

giwonKIM by Associate III
  • 1662 Views
  • 3 replies
  • 0 kudos

dac+timer

void HAL_DAC_ConvCpltCallbackCh1(DAC_HandleTypeDef *hdac){ HAL_GPIO_TogglePin(START_OF_FRAME_GPIO_Port , START_OF_FRAME_Pin);}   uint32_t val[] = { 500, 600, 700, 800, 900, 1000, 1100, 1200, 1300, 1400};   HAL_DAC_Start_DMA(&hdac1, DAC_CHANNEL_1, val...

msg-1001059758846-54432.jpg
nimaltd by Senior
  • 2063 Views
  • 3 replies
  • 0 kudos

U5G9 USBX without ThreadX

CubeMX: 6.11.0STM32U5: 1.5.0uVision: 5.39.0.0Hi, I saw the latest post about USBX baremetal now being possible and thought i would give it a try.I want to read USB drives and usb uart port to PC for comms. but get the following errors in uVision when...

PhilipC_1-1714130818521.png PhilipC_0-1714130748026.png
PhilipC by Associate III
  • 2032 Views
  • 2 replies
  • 1 kudos

Resolved! Update Problem

After STM32CubeMX update from version 6.10.0 to 6.11.0 WorkBench give me and error (see picture Worckbench.jpg attached).How to solve this problem ?I don't find any configuration on Wokbench to specify new STM32CubeMX installation.

UniRob by Associate III
  • 3327 Views
  • 3 replies
  • 0 kudos

Why has CubeMX changed FatFS Version from 0.14 (2019) to 0.12 (2023?). - Which version should I use and why?

Hi,In 2019 I built a project using an SD Card and cube MX built the platform with FatFS R0.14 which came out in 2019.I revisited this project with a view to updating drivers and third party software. To find out what version of FatFs cube was using n...