Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
We are using ST IMU LSM6DSL in to our chipset/PCB.We are looking for ready to use software or algorithm to implement in to our firmware to determine the speed/acceleration & distance from IMU data.Is there any example code available for share?
Hello all, I'm looking at the datasheet for the STW56N60DM2, and it's really not clear if the back of the FET is electrically isolated from the Gate, Source, and Drain. Typically, this is more clear in other datasheets I've looked at. Below is the ...
We got Sensor tile box and they were working fine until we uploaded this:https://www.st.com/en/embedded-software/stsw-mksbox1-bl.html/1000vai bluetooth. Now they are not visible on the app ST ble sensor. How to update the original firmware on the sen...
I struggle to use PDM Filter library.This is the message error I get : What I have done so far are : - in project properties, C/C++ general, Paths and syombols, in "Includes" I added the path to pdm2pcm_glo.h ; in "Library Paths" I added the path to ...
Hello,We have been using the LSM9DS1 in our own design with Linux kernel 4.19.x by adding drivers from ST github, and using the iio_generic_buffer tool to read values.Now we are upgrading to linux kernel 6.1.46 and I have checked that the drivers are...
hiwere would i find a recent webinar on how to use X-CUBE-MEMS1? I am interested in Lsm6DSL.Thx
In the project I use Attiny13a) + LIS2DH SPI interface. One leg of the microcontroller is missing. Is it possible in SPI mode to connect the CS pin directly to GND, and not to the microcontroller port.In I2C mode there are enough pins, everything wor...
HiI am updating a PCB comprised of LSM6DSL, LSM303AGR and STM32F4 for a customer. I wonder if these 2 sensors are still the latest and greatest? Or should I better switch to some thing newer?Thx
Hello there,What is the resonance frequency of the LSM6DSO32 accelerometer and gyroscope?It is not available in the datasheet. I tried to open a customer support tickets but they just forwarded me to this forum.