Skip to main content
Associate
November 28, 2023
Question

How to test the IMP23ABSU MEMS

  • November 28, 2023
  • 1 reply
  • 1324 views

I would like to use the following MEMS microphones to test the resonance frequencies of an ultrasonic bath:

https://www.st.com/en/evaluation-tools/steval-mic007v1.html#overview

I would like to ask what other parts I need to convert the analog signal of these MEMS microphones so that the measurement data can be read out on my PC via USB cable.

Alternatively, could you recommend other MEMS microphones that already have an integrated analog-to-digital converter and are suitable for measuring frequencies in the ultrasonic range (~80 kHz)? What additional components would be required to transmit these signals via USB?

 

Many thanks in advance!

This topic has been closed for replies.

1 reply

Federica Bossi
ST Technical Moderator
December 13, 2023

Hi @EcoKF ,

Welcome to ST Community!

Are you going to put the microphone in water? if yes, this application is not suggested as the device may be damaged by contact with water.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
EcoKFAuthor
Associate
December 14, 2023

Hi @Federica Bossi ,

Thank you for the answer!

The micropone will be placed above the water surface. So it won't be in contact with water.

Federica Bossi
ST Technical Moderator
December 15, 2023

Perfect, I suggest you to combine the STEVAL-MIC007V1 with the X-NUCLEO-AMICAM1 (https://www.st.com/en/ecosystems/x-nucleo-amicam1.html) that is developed to stream audio on USB up to 192kHz (ultrasound band up to 96kHz)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.