SAI with PDM microphone on STM32MP157CAA
Is it possible to use SAI for PDM microphones and ALSA with the current Linux kernel on a STM32MP157CAA SoC?
Is it possible to use SAI for PDM microphones and ALSA with the current Linux kernel on a STM32MP157CAA SoC?
Hello, I'm working on a project involving voice recognition. So, I used the stm32 sensory library to complete this project and the MP23DB02MM digital MEMS PDM microphone. However, I only found one example that used STM32H747I-DISCO, so I ported it to...
I'm trying to implement a 6- or 8-microphone arrangement, as outlined in AN5027 (p25). The recommended approach is to use an SAI with PDM interface, but I'm struggling to find a suitable MCU (and subsequently, a suitable Nucleo dev board). I've not ...
I want to connect a MEMS microphone to my stm32 using its SAI interface. I found a document called "Interfacing PDM digital microphones using STM32 MCUs and MPUs" which gives some examples about how to do it.My question is about the configuration :Wh...
I'm trying to get data from PDM microphone and convert it to PCM data. This is my first project on stm32 and I'm starting to debug the project. Could you take a quick look at my code and say if you notice something wrong ? Some part of the code come ...
I'm trying to get the SAI working in receive mode with a MEMS microphone, but when i try to receive data it only returns 0? Here is the SAI setup:saiHandle.Instance = SAI1_Block_A; // audio block A. saiHandle.Init.Protocol = SAI_FREE_PROTOCOL; sa...
I have a really simple application setup. I'm currently feeding in one PDM microphone. I'm using the SAI interface (code is attached). First there appears to be a bug in the ST code. The SAI_PDMCR register have a field to set up to 4 microphones (see...