MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-STWINBX1: BleSensors App = Cannot Connect via BLE

I recently received the STEVAL-STWINBX1 and plugged it in out of the box and it worked fine.  There was a firmware update which I did successfully. Next, I downloaded FP-SNS-STBOX1 v1.5.0 to test it out.  As per the readme I imported the "STM32CubeFu...

WP by Associate III
  • 568 Views
  • 2 replies
  • 1 kudos

STEVAL-STWINBX1 Data Not Displaying in STBLESensor App

Greetings all,Just received a STEVAL-STWINBX1 multisensor evaluation board and I was able to connect to it through STMCube32Programmer (Win64 version) and am trying to see the real-time sensor data from the iOS app (ST BLE Sensor v5.0.0 on iOS 16.5.1...

DJHyp by Associate
  • 338 Views
  • 0 replies
  • 0 kudos

Resolved! DC bias from MEMS microphone using ADF on STM32U5

I have a MEMS microphone (IM72D128V01, using this eval kit) with PDM output connected to a STM32U5 NUCLEO board.It's connected to the ADF/Audo Digital Filter peripheral which I have configured to provide a 5th order CIC filter with a 32x decimation f...

DGran.3 by Associate II
  • 612 Views
  • 3 replies
  • 0 kudos

How to read Sensor data from STM32U5 ( B-U585IOT02A )

Hello community,I've B-U585IOT02A. I want to use sensor values from it to my application running on node.js. I think to import those sensor values to application over the local network using mqtt. But as their is already a web-server installed in B-U...