MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I want to control same sensor in same I2C Bus.

 I use STM32F401RE nucleo board to detect tilt. I will use same MEMS sensor (ISM330DLC). Three. But I want to control that sensor in I2C1 Bus.  I know setting SA0 to distinguish SAD. it's only possible to two devices.  I need to control three devices...

sonja by Associate II
  • 246 Views
  • 1 replies
  • 0 kudos

Problem with MS5611 Barometer Pressure Reading

Posted on November 28, 2017 at 14:27Hi all! I am trying to read temperature and pressure values (then, convert pressure to altitude) from MS5611 barometer using I2C interface with STM32F4. So far, I managed to read both temperature and pressure valu...

Official library for LIS3DH with FIFO DMA transfer

HI, I am trying to develop a application with a accelerometer over 5kHz.I have some samples of LIS3DH. Does exits any repository of mem senc?I search in cubemx but is not there.I can write the library from datasheet but it is a lot of time and it wil...

tcg by Associate III
  • 1077 Views
  • 6 replies
  • 0 kudos