MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSL Power Consumption

Hello,I am writing a firmware with nrf52832 microcontroller and I have interfaced ST's LSM6DSL module. I am facing some issues regarding power consumption of LSM6DSL module. I have used 10K resistors with sda, scl, sdO and cs pins is this correct.I a...

yash2530 by Associate II
  • 373 Views
  • 3 replies
  • 1 kudos

LSM6DSRX - Repeatable noise on X axis

Hello,I'm working on a project where I use the LSM6DSRX. I have noticed that the Gyro has a strange behavior, reporting peaks on the X axis while the device is solid static. The peaks may be correlated to the temperature change but it's not clear yet...

DUT2.png DUT1.png DUT3.png
Candrian by Associate
  • 165 Views
  • 4 replies
  • 0 kudos

Reset SFLP on LSM6DSV16?

HI,Is there any way to reset SFLP "Game vector" readings at runtime, once SFLP enabled?For instance, after few minutes of SFLP run, it reports (after quaternion to Euler conversion) YAW: 1.5, PITCH: 0.5, ROLL: 0.1. And I'd like to reset Yaw to 0 (zer...

lsm6dsv16x OIS gyro data thru SPI2

Hello experts, I'd like to ask about lsm6dsv16x OIS gyro data thru SPI2.I could successfully read OIS gyro data thru UI, but I couldn't do it thru SPI2.I checked Mode 3 self test part in lsm6dsv16x  app note, but still I got failed.Could you give som...

Mems configuration on Custom Board

Hello,     after experimenting MEMS sensors with the IKS4A1, I developed a custom board based on STM32F407 CPU with the LSM6DSV16XTR accelerometer+gyroscope and LIS2MDLTR magnetometer.The aim is to get board inclination and compass information with t...

MRaff.1 by Associate III
  • 228 Views
  • 2 replies
  • 0 kudos

Design confirmation with the IMU sensor

Hi Team, We have BHI160B BOSCH IMU sensor. We worked on it using STM32L053R8 board. We are able to read the Quaternions and calculating RPY. But now we are finding Yaw drift issue with that IMU. Is there any IMU sensor related to ST that doesn't get ...

VB.4 by Associate II
  • 220 Views
  • 1 replies
  • 1 kudos

Reading SFLP Data from ism330bx

I'm trying to extract the data Game Rotation Data from the ism330bx sensor. I'm just not quite sure, which setting to use for that. What I did so far:Setting the sensor for an ODR of 480Hz with a range of 4000dps and 8g.(ism330bx_reset(NULL)) (ism330...

ritzmo93 by Associate
  • 157 Views
  • 1 replies
  • 0 kudos

STEVAL-MKI245KA IMU readings not updating

I'm using the STEVAL-MKI245KA development kit, trying to get the IMU readings with an AT-Mega through I2C. The I2C communication between the adapter board of the kit is working, but the IMU values recieved by the arduino are not updating. When I run ...

cloudymnms_0-1723222036195.png