MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3 SPI communication problem with STM32F4

Привіт! У мене проблема з отриманням даних із датчика LSM6DS3. Коли я намагаюся прочитати значення реєстру "WHO_AM_I", я отримую надто короткі імпульси у відповідь, які не можуть бути прочитані поданими до його тактового сигналу.Я використовую цю пла...

DmytroMachkovskyi_0-1716675423212.png DmytroMachkovskyi_1-1716676173880.png DmytroMachkovskyi_2-1716676417924.png DmytroMachkovskyi_3-1716676549564.png

Resolved! Unicleo-GUI datalog's timestamp not working correctly

I'm working with a nucleo 401RE and a x-nucleo ISK 01A3 as hardware and algobuilder and unicleo-GUI as software. If I measure, for example, the rotation vector 9X throughout the day and save the output datalog using Unicleo-GUI, the timestamp shows t...

aesteban by Associate III
  • 1398 Views
  • 1 replies
  • 0 kudos

Resolved! Issue while configuring the example of lis2dw12 sensor

HiI am trying to configure the accelerometer sensor to read the data polling  as the example suggested in githubWhen I try to read /* Read output only if new value is available */lis2dw12_flag_data_ready_get(&dev_ctx, &reg);At initial the drdy will b...

M4n0j by Associate
  • 2110 Views
  • 2 replies
  • 0 kudos

Resolved! Getting started with STEVAL-MIC007V1

Hi Everybody, I am a beginner and I need some information to start using the following devices:- Nucleo-F401RE- X-Nucleo-Amicam1- Steval-mic007v1. I have currently downloaded the following material:- X-cube-memsmic1- Link007- Link009- Stm32cubeid.Is ...

OsBo by Associate
  • 1291 Views
  • 1 replies
  • 0 kudos

spi drives mp34dt05 microphone chip and collects PDM data stream

 I now want to use the spi port of the stm32F407 series to collect data from the PDM microphone of mp34dt05. My SPI is set to the main device to only receive. There are SCK and MISO ports. The SCK clock is 2.25Mhz. MISO receives data, but I found tha...

Daqiang by Associate II
  • 3060 Views
  • 2 replies
  • 0 kudos

Power consumption of magnetometer lis2mdl

I used in the past lis2mdl. I need to reproduce the former product. I ordered the same parts but I faced an issue with the magnetometer. The part number is the same but i got different power consumption. I got an image with the different magnetometer...

IMG_20240502_153331.jpg
Kostas_N by Associate
  • 2125 Views
  • 3 replies
  • 0 kudos

Resolved! LSM6DSR Wake Up and Activity Detection

Hello, currently I am using LSM6DSR for developing my apps.I have tested this sensor for Wake Up detection with 218.75 mg threshold and Activity detection with 15.625 mg threshold without any issues.Is it possible to enable both of these detection at...

Unexpected behaviour with LSM6DSO32TR

Hi,We are using an LSM6DSOX IMU and Micron MT29F2G01ABBGDWB Nand Flash on a common SPI bus. We didn't see any issue until we upgraded the LSM6DSOX with an LSM6DSO32. The datasheet suggests that they are drop-in replaceable. Both the flash chip and IM...

UQure by Associate
  • 1670 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.