MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sir i'm trying to communicate LPS25HB sensor with STM32F072RB board please could you try to help me to resolve this issue? I'm giving you brief Details in Details box?

Sir i'm trying to communicate LPS25HB sensor with STM32F072RB board but the sensor is not acknowledging and to make sure i have connected RTC DS3231 it is working properly. I have checked clock speed with 100khz and 400khz also, pull-up i have connec...

VDutt.1 by Associate
  • 216 Views
  • 2 replies
  • 0 kudos

Resolved! What is the accuracy of stm32f070 internal temperature sensor?

Hello,As per page number 17 of datasheet of STM32F070 series we can see that it consists of internal temperature sensor. It's written that with calibration we can get quite accurate value of the temperature but can it be used as replacement of any ex...

JKSah by Associate II
  • 606 Views
  • 3 replies
  • 0 kudos

X-NUCLEO-53L0A1 with Nucleo F030R8

Posted on August 10, 2016 at 16:46Hy,what would be the easiest way to use the VL53L0X Nucleo Expansion board (X-NUCLEO-53L0A1) with Nucleo F030R8?All given examples rely on a F401, the source code would not work immediately, because there are some f...

harald by Associate III
  • 142 Views
  • 1 replies
  • 0 kudos

can iNEMO M1 work with Nucleo board programming?

Posted on January 19, 2018 at 11:22hi everyone,i'm trying to debug my program on the iNEMO M1 but when i press the reset button to start the program the iNEMO is disconnected from the debugger and i can't talk to it anymore, so i can't see where the...