MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST MEMS studio - STEVAL STWINBX1 - Connection error

I'm having problems to be able to establish the connection between STEVAL STWINBX1 and ST MEMS Studio software, with either of the two available ways (BLE or Serial port). In the first case, mainly the board won't be shown to select. In case it does,...

jvf_13 by Associate
  • 502 Views
  • 2 replies
  • 1 kudos

lps33k

helloI'm currently using the LPS22DF pressure transducer, which can withstand up to 22,000 g, but since in the work environment there's dust and water, I'm going to switch to either the LPS28DFW or LPS33K since they're waterproof, but in their datash...

ljm by Associate III
  • 261 Views
  • 0 replies
  • 0 kudos