cancel
Showing results for 
Search instead for 
Did you mean: 

lsm6dsv16bx data validation

Varsha
Associate III

I have integrated lsm6dsv16bx in my Microcontroller and I'm able to see the IMU datas in output for example:  AX=61,AY=-131,AZ=-997,GX=-770,GY=2380,GZ=560.
I have used the example code provided in the ST's official github page(https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lsm6dsv16bx_STdC/examples/lsm6dsv16bx_read_data_polling.c).
I'm able to see the changes in output during movement, & there seems to be less change in output while the sensor is static.
The thing is, how can I confirm if this value that i'm getting is correct/accurate? is there any way to confirm/evaluate this value?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Varsha ,

There aren't reference values to share because it depends on the position of the device and there is also a piece to piece variability.

I did a short acquisition keeping the sensors in a steady position on my desk and I obtained these values:

A_X [mg]   A_Y [mg]   A_Z [mg]  G_X [dps]   G_Y [dps]   G_Z [dps]   
48.068 -25.925 1031.33 -0.18813 0.34125 -0.14438  
50.142 -26.474 1030.66 -0.1575 0.328125 -0.17938  
50.447 -26.169 1029.86 0.0175 0.214375 -0.24938  
54.168 -27.267 1030.35 0.065625 0.406875 -0.16188  
49.41 -23.241 1032.24 -0.04375 0.55125 -0.1575  
51.179 -25.376 1030.41 -0.0875 0.39375 -0.10063  
50.142 -25.742 1034.38 -0.07438 0.441875 -0.13125  
50.874 -27.572 1028.15 -0.10063 0.450625 -0.20125  
51.362 -22.875 1031.2 -0.10063 0.42 -0.21438  
48.007 -25.376 1028.4 -0.09188 0.573125 -0.175  
49.288 -24.461 1030.17 -0.16625 0.4725 -0.15313  
51.789 -27.45 1031.69 -0.0175 0.240625 -0.19688  
53.741 -28.731 1030.9 0.231875 0.205625 -0.28  
50.203 -24.156 1029.98 0.16625 0.310625 -0.11813  
48.922 -27.328 1030.6 -0.07875 0.30625 -0.10063  
50.02 -30.073 1028.09 -0.07438 0.30625 -0.17938  
51.24 -26.474 1026.93 0 0.240625 -0.23188  
50.63 -25.376 1032.97 -0.28438 0.188125 -0.23625  
48.922 -29.28 1031.63 -0.49438 0.16625 -0.28  
47.641 -28.67 1029.92 -0.2975 0.25375 -0.21  
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
Federica Bossi
ST Employee

Hi @Varsha ,

Which is the unit of those values? LSB? And which is the FS and ODR you set?

By the way, seeing some fluctuations when the device is static is normal, it could be due to vibrations from the environment for example.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@Federica Bossi unit of those are mg & mdps. 
For accelerometer full scale is set to 2g, & odr is set at 1920Hz.
For gyro full scale is set to 2000dps, & odr is set at 1920Hz

Federica Bossi
ST Employee

Hi @Varsha ,

I confirm you that your values are reasonable, the Y gyro axis is a little bit high but it could be due to the position of the device.

Hope this helps.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@Federica Bossi Thank you!
Could you please let me know the procedure / known reference values to validate and calibrate the data?

Hi @Varsha ,

There aren't reference values to share because it depends on the position of the device and there is also a piece to piece variability.

I did a short acquisition keeping the sensors in a steady position on my desk and I obtained these values:

A_X [mg]   A_Y [mg]   A_Z [mg]  G_X [dps]   G_Y [dps]   G_Z [dps]   
48.068 -25.925 1031.33 -0.18813 0.34125 -0.14438  
50.142 -26.474 1030.66 -0.1575 0.328125 -0.17938  
50.447 -26.169 1029.86 0.0175 0.214375 -0.24938  
54.168 -27.267 1030.35 0.065625 0.406875 -0.16188  
49.41 -23.241 1032.24 -0.04375 0.55125 -0.1575  
51.179 -25.376 1030.41 -0.0875 0.39375 -0.10063  
50.142 -25.742 1034.38 -0.07438 0.441875 -0.13125  
50.874 -27.572 1028.15 -0.10063 0.450625 -0.20125  
51.362 -22.875 1031.2 -0.10063 0.42 -0.21438  
48.007 -25.376 1028.4 -0.09188 0.573125 -0.175  
49.288 -24.461 1030.17 -0.16625 0.4725 -0.15313  
51.789 -27.45 1031.69 -0.0175 0.240625 -0.19688  
53.741 -28.731 1030.9 0.231875 0.205625 -0.28  
50.203 -24.156 1029.98 0.16625 0.310625 -0.11813  
48.922 -27.328 1030.6 -0.07875 0.30625 -0.10063  
50.02 -30.073 1028.09 -0.07438 0.30625 -0.17938  
51.24 -26.474 1026.93 0 0.240625 -0.23188  
50.63 -25.376 1032.97 -0.28438 0.188125 -0.23625  
48.922 -29.28 1031.63 -0.49438 0.16625 -0.28  
47.641 -28.67 1029.92 -0.2975 0.25375 -0.21  
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.