MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

H3LIS331DL

Hi,I readed the default value of the identification register in H3LIS331DL by SPI mode and it responded with 0x32h as per the data sheet,but while reading the STATUS REG default value it responded with 0xFFh instead of 0x00h. How it's possible one re...

Gokulraj by Associate II
  • 307 Views
  • 2 replies
  • 0 kudos

Possible bug in Unico GUI v9.13.0.0

Dear ST Community,Have no experience with STM32 MCUs nor with any programming IDEs used to develop for STM chips. As i am developing on espressif MCUs...However recently i am trying to integrate a MEMS sensor of STM into my project.I found out Unico ...

RDyla.1 by Associate
  • 305 Views
  • 3 replies
  • 0 kudos

Resolved! bug report [cubeMX] Makefile gen

i'm a linux user, so i use cubeMX gen a code framework with project type: Makefilesnow, i try to use x-mems lib, the makefile is miss a ":" that lead "make" command error.after add the colon, seems goodFYI

0693W000004I5N2QAK.png
MMa.1893 by Associate III
  • 241 Views
  • 1 replies
  • 0 kudos