MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use STEVAL-MKI109V1 command in terminal ?

Posted on August 27, 2014 at 08:35I want to utilize command in STEVAL-MKI109V1 board.  STEVAL-MKI108V1 is insert on the  STEVAL-MKI109V1 board, I utilize user guide to set up. Bur terminal can't receive any data? How do I slove the problem? #mki1...

LIS2DH Digital data readout conversion to G

Posted on September 05, 2014 at 16:24 I'm struggling to understand the correct method/formula to convert the digital reading of the accelerometer to G units (LIS2DH). The data sheet states that The value is expressed as two’s complement left just...

fleming by Associate
  • 862 Views
  • 0 replies
  • 0 kudos

LIS3MDL offset

Posted on July 09, 2014 at 15:47I received some results from LIS3MDL.I tried to measure the magnetic field of the Earth = 0.05 mT = 0.5gauss. Full scale setting = �4gauss. If I rotate the magnetometer Y axis towards the north I receive 0xF3E0 (-3104...

glory_man by Associate II
  • 1230 Views
  • 1 replies
  • 0 kudos

LPY410AL Drive Strength

Posted on August 28, 2014 at 19:21I have a question pertaining to the drive strength of the analog outputs of the LPY410AL 2-axis analog gyroscope. The circuit is as follows: The analog outputs of the LPY410AL are connected to the inputs of a LMV324...

LIS331dlh I2C read problem

Posted on August 21, 2014 at 14:11Hi!I am using the LIS331DLH sensor in my project. I have no problem with processing between CPU and sensor via SPI. But I cannot communicate them via I2C - all registers are return 00 when reading.Here is the part o...

Using LIS331EB

Posted on August 12, 2014 at 12:51Where can  I find  all additional files for IAR (startup_lis331eb.s, StdPeriph_Driver, StdPeriph_Examples )? Should I use core_cm0.h or you can give me something like lis331eb.h? Thanks for the help. #lis331eb

ridelar by Associate
  • 821 Views
  • 0 replies
  • 0 kudos

LSM303DLHC reading 0x00 when enable both acc & mag

Posted on August 11, 2014 at 19:30 Hello, recently i started working on a project using LSM303DLHC, i noticed if i enable both accelerometer and magnetometer, i get 0x00 data. If i enable only the accelerometer, the data is normal on all three axis ...

Bogdan by Senior
  • 757 Views
  • 0 replies
  • 0 kudos