MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error in Reading temperature using Lis3dh

 Hi everyone, I have an STM32L4 series-based board with an embedded LIS3DH sensor. I've written code to read temperature values from it, configuring all settings as per the datasheet. However, I'm having trouble obtaining the exact temperature value ...

AKH by Associate
  • 105 Views
  • 1 replies
  • 0 kudos

Resolved! Behaviour change when powering with external power source

Hi everyone,I am using a STWINKT1B and I am trying to evaluate its power consumption while operating. The Wifi communication always works well when I power the board by the battery or the USB port but never when I plug it to my voltage source (5V on ...

chhhhak by Associate II
  • 526 Views
  • 6 replies
  • 0 kudos

Using LIS25BA with STM32L4 Nucleo Board

I am using STM32L452RE Nucleo Board and LIS25BA module.I2C works fine. I wish to get accelerometer data through TDM now. I am unable to do so. For now, I am using polling mode. The code I am using is given below and the SAI configuration I am using i...

Arka by Associate
  • 389 Views
  • 2 replies
  • 0 kudos

Resolved! (SOLVED) SPI communication problem with sensors

I'm using STEVAL-STWINKT1 (MCU STM32L4R9ZIJ6) and I'm trying to communicate with the motion sensors (ISM330DHCX, IIS3DWB, IIS2DH) by SPI3 interface (polling). I wrote a code very similar to that one present in the "Serial_DataLog" project, using HALs...

irene by Associate II
  • 978 Views
  • 7 replies
  • 0 kudos