MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Saturated data on STwinkT1B with the iis3dwb sensor

Hello,For a predictive maintenance project on an STwinkT1B board. I am using an iis3dwb vibration sensor.When retrieving the data provided by the sensor, one of the obtained values is saturated close to 65535, which is close to 16 bits.I am using the...

RaphaelP by Associate
  • 349 Views
  • 1 replies
  • 0 kudos

Resolved! SensorTile MEMS Audio stream to Unix-like OS (Raspbian)

I am exploring the SensorTile (STEVAL-STLKT01V1) and would like to capture Audio recordings on a Unix OS (namely Raspbian). I have looked through the documentation here and the option to save audio to SD card is not ideal for my application, neither...

SensorTile.box USB connection does not work.

I am trying to work through the labs from the recent ST sensors workshop. The very first step in the Pro-mode lab is to enter the DFU mode and program the SensorTile.box with a precompiled image. The problem is that when I connect the tile to my co...

Rita Ch. by Associate II
  • 1000 Views
  • 4 replies
  • 0 kudos

STM32F072 usb audio

Posted on May 19, 2016 at 04:45 Hi guys, I new to STM32, was mostly use PIC32 for USB audio application but due to cost decided to switch to STM Now I have STM32F0 discovery board with STM32F072RBT6. I tried to setup USB audio w...

sgpiqx by Associate II
  • 1639 Views
  • 9 replies
  • 0 kudos

Audio Playback and Record project using CooCox IdE

Posted on August 10, 2016 at 16:45I have downloaded STM32F4-Discovery_FW_V1.1.0 firmware package and want to use the example of Audio Playback and Record on STM32F411.I am facing a lot of problems in building the project itself such as C:\CooCox\CoI...

jainpl15 by Associate
  • 486 Views
  • 0 replies
  • 0 kudos

Mems microphones frequency response

Posted on September 28, 2015 at 16:38Hello,I�m using an stm32f4-discovery board and I�m trying to sample the on board mems microphone at 48 kHz. I record a large number of samples and send them to the computer via USB (if someone knows a better way ...

rjrg1989 by Associate
  • 503 Views
  • 2 replies
  • 0 kudos