| Subject | Author | Posted | |
|---|---|---|---|
|
We had three Sensor TileBox units. In an interesting morning of work, I got the one I have in the U...
| 2026-05-02 1:10 PM | ||
|
Hello, For the ASM330LHH, it's not clear which registers are covered by the BDU setting. Although...
| 2026-05-01 12:59 PM | ||
|
Hello, I know there are already other threads on this topic, but none of the replies have convin...
| 2026-04-30 3:26 AM | ||
|
Hello everyone, I'm working with the LIS2MDL sensor (steval_mki181v1) , i made a connection betwee...
| 2026-04-27 7:11 AM | ||
|
Hello, I intend to put LIS3DH and LSM6DSV32X on same SPI bus and use different CS lines to address...
| 2025-12-30 3:56 AM | ||
|
On platforms like LCSC and Mouser, an IMU labeled "LSM6DSVQTR" is listed separately from the LSM6DS...
| 2025-12-26 3:01 PM | ||
|
Now I am working on my own project which involve with detecting the pattern of hand gestures using ...
| 2025-12-11 6:40 PM | ||
|
We have integrated LSM6DSV16X (IMU) and ISM303DAC (magnetometer) on Android 10 running on the NX...
| 2025-11-19 5:28 AM | ||
|
Dear ST, I am working with the STHS34PF80 PIR sensor on an i.MX8MP platform, using the upstream-st...
| 2025-09-18 2:27 AM | ||
|
I am using the MLC of the LSM6DSOX along with the Nucleo-L432KC. I am using the .h file generated f...
| 2025-09-10 8:05 AM | ||
|
Hey ST Community, I'm currently trying out the CCA02M2 MEMS microphone board on a NUCLEO-L476RG, u...
| 2025-08-18 11:55 PM | ||
|
I am using the STHS34PF80 sensor (SparkFun Presence Sensor - STHS34PF80) with an ESP32 in my ceilin...
| 2025-08-17 11:35 PM | ||
|
Hello, I'm working on an IMU project. I need to measure pitch/roll/yaw rotation in quaternions. F...
| 2025-08-11 5:24 AM | ||
|
Hi, I’m using the NUCLEO-STM32F401RE with the X-NUCLEO-CCA02M2 board, which has two MP34DT06 PDM m...
| 2025-08-06 12:20 AM | ||
|
Hi ST guys, I played with the LIS3DH accelerometer options and don't really see difference in inte...
| 2025-07-31 8:04 AM | ||
|
Hi, I am follow up on the query i am posted "https://community.st.com/t5/mems-sensors/integratin...
| 2025-07-29 10:35 PM | ||
|
Hi, I am using LSM6DSO as my I3C sensor. It works well with RSTDAA and ENTAA. But when I tried to g...
| 2025-07-29 2:01 AM | ||
|
Dear all, I am using SensorTile.box STEVAL-MKSBOX1V1 with St app. I made application with vibrome...
| 2025-07-25 2:09 AM | ||
|
dear all, i want to recoed acceleration date from LSM6DSOX . i made app on st app and made output...
| 2025-07-23 9:15 AM | ||
|
Hi, I have a compulab SBC (UCMiMX8Mplus sbev) it is a dev kit. I am connecting the STEVAL-55GMB...
| 2025-07-17 7:48 AM |