MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Actual Detection Range and FOV of STHS34PF80?

Hello everyone,I’ve been working with the STHS34PF80 sensor and would appreciate some insights regarding its detection range and field of view (FOV). In my tests, I’ve observed that the sensor detects presence effectively up to a range of about 1 met...

mobaid by Associate III
  • 140 Views
  • 2 replies
  • 0 kudos

ILPS28QSW Gel Info

Hello all,I am looking for more info on the gel used with ILPS28QSW.We want to use it in an application where the sensor may be submerged in 10% to 40% alcohol v/v for extended periods of time. Will the sensor be okay? Or is there another product whi...

STHS34PF80 Sensor's Power Consumption is very high.

Hello there, I am currently working on a project where I am prototyping STM32WL55 with an STHS34PF80 sensor to detect the presence. The presence detection is excellent and robust so far. However, the power consumption seems to be very high at the mom...

STHS34PF80 Abnormal operation

When STHS34PF80 detects the human body for a period of time, TPRESENCE cannot fall back normally, and pres_flag is always 1。 code:

top_0-1711014368016.png
top by Associate
  • 460 Views
  • 3 replies
  • 0 kudos