MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi everyone, I'm trying to acquire a temperature from a MCP9808 sensor with a B-L072Z-LRWAN1. But I got an "onRxTimeout" error everytime I try. Is someone knows why ? Thank you a lot for helping me.

 I'm using stm32cubeIDE and I got nothing more than the STM32CubeExpansion_LRWAN_V1.2.1's libraries (stm32l0xx_hal_i2c) to help me. I'm on the i2c1 interface on PB8 and PB9 ports. I think the problem is that I don't know how the flags works.

YMAIL by Associate II
  • 345 Views
  • 5 replies
  • 0 kudos

VL53L1X range readings not accurate after 200cm

We are testing VL53L1X Time of Flight Sensor with STM32L072(B-L072z-Lrwan) controller. Within 200cm the range measured by sensor is accurate. After 200cm we are getting a lot of variation in the range is measured by the sensor. We have to change the ...

VL53L1X Issue

Posted on June 28, 2018 at 09:00HiI am facing issue while taking multiple readings for averaging in the VL53L1X sensor.Our sensor is interfaced with B-L072Z-LRWAN1.We are not getting consitent reading as shown below:2486249024892490248724882490Above...

VL53L1 Accuracy Issue

Posted on June 19, 2018 at 14:12HiWe have interfaced VL53L1 to STM32L0 EVM board(B-L072Z-LRWAN1).We tested the sensor with a white surface and water in opaque object.The accuracy with white surface are good if the object is below 200cm.If above 200c...

Voltage drop when connecting IKS01A2 to B-L072Z-LRWAN1

Posted on April 03, 2018 at 18:10So the B-L072Z-LRWAN1 board is configured to be powered through the 3.3V pin by removing SB6 and R26. Furthermore, the ST-LINK was disconnected by removing SB28, SB29 and SB37. When testing with some example code and...