Auto detect budrate serial
Posted on June 28, 2016 at 11:48Hello,I have a STM32L031K6 and I want some auomatiser my reception function is adding automatic detection of transmission speed (baud rate) how I can do. thank you very much
Posted on June 28, 2016 at 11:48Hello,I have a STM32L031K6 and I want some auomatiser my reception function is adding automatic detection of transmission speed (baud rate) how I can do. thank you very much
Posted on May 24, 2015 at 18:38Hello All, 1) how can I have an asynchonous Transmit command ? 2) what is the largest amount of data I can put into CDC_Transmit_FS ? I am implementing CDC on my firmware based on CubeMx. So far it works (I have to inc...
Posted on October 14, 2015 at 18:13after few frequent connects and disconnects, the program fails to detect pendrive connection/disconnection. Is there any minimum duration required between connection and disconnection.??i am working with STM32f205 ...
Posted on July 03, 2014 at 12:01Hello,I'm using STM32CubeMX to generate a project for STM32F207 that uses USB Host. The project compiles without problems. I have a custom USB device that uses CDC to send and receive serial data. When the device is a...
Posted on July 29, 2015 at 14:50Why is it not possible to choose Custom HID class for STM32F2 in CubeMX?The selection is grayed.Regards,Paul #cubemx #hid #stm32f2
Posted on May 26, 2015 at 04:35Hi All,I have generated code for a USB HID device, but it does not do anything, I mean my PC does not recognize anything. I have not changed anything in the code because I was assuming that it should at least get detec...
Posted on February 12, 2015 at 08:50any idea?Regards #usb #cubemx #cdc #stm32
Posted on October 27, 2014 at 00:34I am trying to get a USB CDC Device demo working on an STM32F4 Discovery board (with the STM32F407) with code from the STM32CubeMX generator application. The process has been murky at best, hopefully one of you can...
Posted on September 02, 2014 at 11:22I'm using STM32Cube to generate simple USB MSC project. I'm using STM32F417VG.So I'm selecting USB_OTG_FS - Device_only and USB_DEVICE - Class For FS IP - Mass Storage Class. Then I'm generating source code, comp...
Posted on April 08, 2014 at 11:51 Hi, I can't get the USB Host code generated by STMCube to work. When I connect a device, none of the interrupts get triggered - the software doesn't seem to recognize it at all. The peripheral cl...