STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Resolved! power consumption calculator for stm32h7

Posted on October 17, 2017 at 22:27Hello,I am trying to estimate power consumption on the stm32h7. The use case i am interested in is sampling 6 channels using ADC3 and transferring the sampled data to memory using BDMA, all this while D1 and D2 dom...

STMCubeMX repository folder

Posted on October 10, 2017 at 23:15I know it's kind of stupid. But I still want to make sure if the repository folder can be changed? Because the capacity of my C is not big enough.#stmcubemx

Simulink model sample time vs. STM32 MCU clock configuration

Posted on November 07, 2017 at 12:53Hello everyone, In this project I just want to use the user button to toggle a LED on my board. The model is designed by using Simulink and initialization codes are generated by STM32CubeMX. During the experiment...

0690X00000608rqQAA.png 0690X00000608sFQAQ.png
Sam Q. by Associate III
  • 2239 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F407G-DISC1 : not listed in STM32CubeMX

Posted on November 02, 2017 at 14:15Hello,I'm new to this exiting world of MCUs.I tried many installs from scratch, did all the available updates I found, but I still can't see my 'STM32F407G-DISC1' in the list of boards in STM32CubeMX.I find 2 'STM...

Resolved! MCU initialization fail while using HSE?

Posted on November 02, 2017 at 18:18I am using NUCLEO-F767ZI board where I observe that when I use the internal clock (HSI), the mcu runs fine, but when I configure the cubeMX project to run on external 8MHz clock (HSE), the mcu fails to run. Follow...

0690X00000608o4QAA.png 0690X00000608ikQAA.png

FLASH_WaitForLastOperation CubeMx error

Posted on January 23, 2017 at 10:02The latest Version of CubeMx (4.19.0) the 'FLASH_WaitForLastOperation' function causes errors if the HAL_GetTick() function is near its rollover point. The cause seems to be 'uint32_t timeout = HAL_GetTick() + Time...

Resolved! Bug report: STM32CubeMX 4.23 MX_RTC_Init

Posted on October 26, 2017 at 10:35Today I have just updated my STM32CubeMX to the 4.23 version.I migrated the project I am using currently. It uses a STM32F767VITx. So far, I was using the 4.21.1 version of STM32CubeMX.Today I made some changes in ...

0690X00000608lEQAQ.png

Resolved! Bug when creating STM32L4 based projects using CubeMX

Posted on July 21, 2017 at 11:02I am trying to create a project for either the L469 Discovery or Nucleo-144 board using CubeMX.My setup is the following:CubeMX 4.22.0L4 Firmware v1.8.1Using STM32 AC6 latest versionIt appears as though CubeMX does no...

Ant M by Associate II
  • 2500 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F746 CubeMX clock not reporting correctly?

Posted on October 25, 2017 at 18:38I'm using an STM32F746VGT6 microcontroller configured from STM32CubeMX for all the clocks and I'm getting roughly 220% higher clock rates reported for SystemCoreClock when compiled. For instance I have an HSE cryst...

0690X00000608kWQAQ.png