STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1591 Views
  • 0 replies
  • 2 kudos

Example code for stm32f4 SD card read via SPI

Posted on February 20, 2018 at 11:27Hi,Kindly help me to find out the example code for read/write the SD card via SPI. I am trying to write or copy the files both USB disk and/or SD card. Please advice.https://community.st.com/tags♯/?tags=stm32f4%20...

When will CMSIS-FreeRTOS be upgraded to v2?

A while back, I found a bug in the osTimer implementation (relating to the callback parameter), and reported it here:https://github.com/ARM-software/CMSIS-FreeRTOS/issues/9only to discover it has been fixed in v2 and the version that ships with the S...

Freetros+Sdio+Fatfs Problem

I try enable sdio+fatfs without freertos and every things work fine.when i enable freertos+sdio+fatfs , my fatfs doesn't work.I enabled Dma.(stm32f4cube_v_1.23)(cubemx 5.0.1)(stm32f407zg)

Example application flashing

I want to flash STM32Cube_FW_F4_V1.23.0 example application code on STM32f429 Nucleo 144 board using eclipse IDE this work with the systemworkbench.How use STM32CubeMX with eclipse ?

chum by Associate II
  • 847 Views
  • 1 replies
  • 0 kudos

STM32CubeMX 5.0 Bug? True Studio can't compile generated project

Hello everyone.I've expirienced an interesting problem today.I've created simple project for STM32F407: just RCC, SW Debug, and couple GPIO Pins (3 for EXTI, 4 for output).But, when I generate project from this file to TrueStudio format, it falls dow...

zedeg by Associate III
  • 2072 Views
  • 2 replies
  • 0 kudos

CubeMX created Custom HID code does not enumerate

I have used CubeMX to create the exact same project starting with basic board Nucleo L496ZG but varying the USB device middlewares for CDC, HID and Custom HID. The CDC and HID examples enumerate 'out of the box' in windows. The custom HID does not. W...

fredferd by Associate II
  • 785 Views
  • 0 replies
  • 0 kudos

STM32F401 FATFS + USB HOST MSC Error.

Hi.I am trying to save .txt files to USB memory with USB HOST MSC and FATFS to STM32F401RB.STM32F4-DISC and examples.So I wrote the code with reference to CUBEMX and the examples I searched.I entered USBH_Path in the * path of f_mount.However, an err...

SWoon by Associate II
  • 1405 Views
  • 2 replies
  • 0 kudos

STM32CubeMX 5.0.1 won't Generate Code

Hi,We are trying to evaluate STM32CubeMX, I can launch it and use it normally, but I have some troubles: it won't generate code when clicking "Generate Code" button. Instead, it produces this error and doesn't do anything more: "Exception in thread "...

XI by Associate
  • 704 Views
  • 0 replies
  • 0 kudos