STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1628 Views
  • 0 replies
  • 2 kudos

Resolved! Bug STMF1x CubeMX I2C Slave Address

When setting the primary slave address for I2C in cubeMX for the STM32F1xxThe generated code will be the address * 2. This created address is incorrect. The address should not be multiplied by 2.for example: Set I2c Slave address to 0x50Generated cod...

neovius by Associate
  • 1904 Views
  • 3 replies
  • 0 kudos

STM32CubeMX USB Mass Storage template

Hi all, I'm trying to set-up a simple USB read/write on our STM32F746G-Disco board using the FullSpeed OTG... but so far it seems that the code generated by CubeMX does not really work...If I'm not wrong, CubeMX in case of USB MSD enable the DMA te...

iw2lsi by Associate III
  • 1891 Views
  • 3 replies
  • 0 kudos

SDMMC: auto card detect?

In CubeMX when choosing fatfs middleware it seems to require a gpio pin. Is that just a limitation in CubeMX? Basically is there a reliable software card detect mechanism using the existing SDMMC lines (4 pin SD card) or must an extra gpio pin be use...

fredferd by Associate II
  • 1548 Views
  • 1 replies
  • 0 kudos

Problem with USART baudarte on STM32l4R5ZIT

Dear all,I'am using a Nucleo-L4RZi with the STM32l4R5ZIT in combination with the software OPENSTM with STM32CubeMX plugin. Thy system clock is 120MHz, same thing for the USART clock.If I set a baudrate of 460800 on the LPUART1, all works correctly. I...

AVagh by Associate II
  • 1144 Views
  • 1 replies
  • 1 kudos

Resolved! STM32CubeMX 5.0.1: LPUART1 missing NVIC menu

I migrate my CubeMx project that is based on stm32l072cbtx to version 5.0.1 but in connectivity menu, LPUART1 NVIC settings doesn't appear. So I can't enable LPUART1 interrupts with code generation. Is there any problem? or I've missed something

0690X000006DiEMQA0.jpg

Different application-speed after download

Hello,I'm using a STM32L433CCU3 in my Application with STM32CubeMX.I'm download my hex-files with the STM32CubeProgrammer in UART serial download mode.If I start my application directly after download with the "Run after programming"-function of the ...

CubeMX deficiency: LwIP DCHP host name hard-wired

Using FreeRTOS + LwIP 2.xIn the generated file ethernetif.c you have:err_t ethernetif_init(struct netif *netif) { LWIP_ASSERT("netif != NULL", (netif != NULL)); #if LWIP_NETIF_HOSTNAME /* Initialize interface hostname */ netif->hostname = "l...