STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1567 Views
  • 0 replies
  • 2 kudos

Resolved! Configuration Window needs to be scrollable

I'm using STM32CubeMX 5.0.1 for creating projectsWhile configuring GPIO using configuration window the properties windows on the bottom of selected GPIO pin overrides the visibility of other GPIO pins at the bottom on configuration window It is not s...

Path name / Display / package link many things to fix

Hi all,Just upgrade to CubeMX v5.1 (from 4.xx) and just to give you feedback:Code Generation Error:"The Code is successfully generated under PATH but MDK-ARM V5project generation have a problem" This is due to "[" and "]" in my PATH. This was not an ...

Thomas LB by Associate III
  • 706 Views
  • 0 replies
  • 0 kudos

Resolved! Bug with L4's Low Layer RTC month macros

#define LL_RTC_MONTH_JANUARY (uint8_t)0x01 /*!< January */ #define LL_RTC_MONTH_FEBRUARY (uint8_t)0x02 /*!< February */ #define LL_RTC_MONTH_MARCH (uint8_t)0x03 /*!< March */ #define LL_RTC_MONTH_A...

Bug with choice legacy library and new CubeMx?

I’m using:CubeMX v5.0STM32F105RCTxHAL_API_version 1.6.1And I have a compilation errors.This happens because CubeMX generates a CAN_InitTypeDef structure for new libraries (version 1.7.0).See what should be the structure for libraries 1.6.1I noticed s...

0690X000008AX7cQAG.jpg 0690X000008AX8BQAW.jpg

Resolved! using SPI to read register value

Hello GuysI am asking you kindly your help.I am trying to read register data from the LSM6DS3 IMU sensor from STM using SPI. I succeeded reading the value 0x69 from register WHO_AM_I using Arduino.Now I am stuck when trying to do it with STM32 micro-...

0690X0000089wYGQAY.jpg 0690X0000089wYQQAY.jpg
moha by Associate II
  • 5183 Views
  • 4 replies
  • 0 kudos

Double signal on PWM driven by DMA

Just trying to set PWM with DMABuffer which I try to use as duty cycleuint16_t BUF_DMA[6] = {3, 4, 2, 7, 9, 1}; PWM is started by buttonHAL_TIM_PWM_Start_DMA(&htim1,TIM_CHANNEL_4,(uint32_t*)&BUF_DMA, 6);Output I getI can't understand why BUF_DMA[3] ...

0690X000008AUpHQAW.png

Mounting USB using fatfs

Hi all,I am having troubles mounting a USB using the "f_mount" function in the fatfs library. My usb does mount but only after many attempts, using a simple counter I have found it to be 81, every single time I run the code it is the same amount of a...

Usb otg conflict with i2c on stm32f4 board?

I have the stm32f429 discovery board and I'm experiencing a conflict between the usb otg hs and the i2c3. I use the cdc usb library which when initialized on it's own works fine as a virtual com port and I can communicate in windows. When any other c...

KGon by Associate
  • 1285 Views
  • 1 replies
  • 0 kudos

Wave generation of particular frequency.

By using timer I want to generate a wave of 27Mhz frequency. Present time I can generate only 13.48khz frequency wave. My timer settings are below please tell me how can I generate it.static void MX_TIM2_Init(void){ TIM_ClockConfigTypeDef sClockSourc...

LACTIC by Associate II
  • 3695 Views
  • 8 replies
  • 0 kudos