STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1626 Views
  • 0 replies
  • 2 kudos

STM32 Discovery Board Code Generation Problem in STM32CubeMX.

I am actually facing issue in generating the code in STM32CubeMX, seems "STM32Cube FW_F4 V1.24.1" is not available for proper code generation.When I try to download "STM32Cube FW_F4 V1.24.1" I am facing repeated issue. please see the issue screen sho...

HArch by Associate
  • 1513 Views
  • 1 replies
  • 0 kudos

Error when generating STM32CubeIDE project

Hi!When I tried to generate STM32CubeIde project, an error occurred:searchjar length = /home/juraj/Programy/STM32CubeMX/third_parties_plugins/array = com.st.stm32cube.ide.common.services.mx.jar-0.0.9.jarsearchjar path = /home/juraj/Programy/STM32Cube...

USB Serial firmware example for STM32F303CBT6?

Is there example code for using the Virtual Port Com from CubeMX?(Determine baud, rxchar, txchar [preferably with DMA], CD, etc)I found this: https://damogranlabs.com/2018/02/stm32-usb-cdc/and it looks like a good starting point, but even though I ca...

TJohn.14 by Associate II
  • 1428 Views
  • 1 replies
  • 0 kudos

USB CDC won't talk to PuTTY

Background: Quick USB stack test on Nucleo F429 with CubeMX-generated USB CDC stack.Added one line to echo input in CDC_Receive_FS (example here: https://damogranlabs.com/2018/02/stm32-usb-cdc/)Windows 10 PC sees virtual COM7 port (usual ding-****, s...

osSignalSet+FreeRTOS Problem

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim){ /* USER CODE BEGIN Callback 0 */  if (htim->Instance == TIM1) {  osSignalSet(defaultTaskHandle, 0x0001); } /* USER CODE END Callback 0 */ if (htim->Instance == TIM4) {  HAL_IncTick(); } /* ...

km naxin by Associate II
  • 986 Views
  • 1 replies
  • 0 kudos