STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1580 Views
  • 0 replies
  • 2 kudos

Unable to add extension package to CubeMX

Hello,I'm unable to install X-CUBE-NFC3 and X-CUBE-IAP-USART extension packs to my CubeMX 5.2 installation. I'm using a downloaded zip and I get this error:What should I do to resolve this? Thanks!

0690X000008jEmBQAU.jpg
Ankit by Associate II
  • 763 Views
  • 0 replies
  • 0 kudos

Best resources to learn FreeRTOS STM32CubeMX & TrueStudio

Hello,I'm rather new at MCU programming but have been a SWE for 20+ years working in low-level Linux (libraries and device drivers) and I understand the basics of multi-threaded programming. I have several STM32 eval boards including P-Nucleo-STM32WB...

STM32F439 delay required before sending packets in LWIP

I am using the ethernet and lwip drivers provided by the STM32CubeMX software on a nucleo-144. I have a program, which upon start, sends out a UDP packet. I set the program to soft reset after a few seconds to characterize this issue. Using a GPIO li...

USB Battery charging bug on cube L4 1.14

HiSeems the new cube L4 package has some updates on the USB driver. The Battery charging functionality no longer works because the BCDEN bit is never enabled in the `HAL_PCDEx_ActivateBCD` function. In the screenshot, left is the previous version of ...

0690X000008j8WpQAI.png

Capture compare interrupt STM32F7 TIM3

Hello there.I have an encoder connected to timer 3 (TIM3) and I'd like to set this timer to generate an interrupt when a certain amount of ticks have been reached (1658 ticks). I'd like to program the timer's counter to 1658 ticks and let the encoder...

SBrid by Associate II
  • 1534 Views
  • 3 replies
  • 0 kudos

CubeMX-5.1.0 fails to install on fedora 29

When I try to installcubeMX on my fresh installed fedora 29, I get following error messages:[sage@linux cubeMX]$ ./SetupSTM32CubeMX-5.1.0.linux chdir /home/sage/Downloads/cubeMX/.current dir /home/sage/Downloads/cubeMXMar 22, 2019 6:06:24 PM INFO: Lo...

MHein by Associate II
  • 1541 Views
  • 2 replies
  • 0 kudos