STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1450 Views
  • 0 replies
  • 2 kudos

Resolved! Creating STM32N6 ioc project for hexaSPI and octoSPI.

Hello,While creating a project for STM32N6 I can’t find the option for hexaspi or octospi for STM32N657B0HxQ . Is there any particular option I have to enable?I am trying to generate the ioc similar to STM32N6570-DK board .I am on 6.15.0 STM32CubeMX....

darla14_0-1758621776963.png
darla14 by Senior
  • 1081 Views
  • 5 replies
  • 2 kudos

Resolved! STM32F070 APB1 clock can't be configured with HSI clock

Hi,APB1 clock can't be enabled if HSI clock is chosen. It says that the driven clock must be 10M<=x<48M, so, without using the PLL it's impossible to get the 10MHz. Things get worse when I try to feed the PLL from the HSI: it says that the PLL should...

Captura de pantalla de 2025-09-20 00-08-43.png 20250919_235605_1758347808903.jpg Captura de pantalla de 2025-09-20 00-24-25.png
XR.1 by Senior
  • 830 Views
  • 2 replies
  • 1 kudos

Resolved! STM32 Cube MX STM32U535 ADC Error

Hi,Running STM32MX Tool 6.15.0 On Windows 10.Started a project for a STM32U535CCTx.I've enabled ADC and configured channel IN8. The software thinks this is connected to PA4, but the datasheet says it is connected to PA3. See screen caps below. Regard...

jminack_0-1757905070998.png jminack_1-1757905125016.png
jminack by Associate II
  • 938 Views
  • 6 replies
  • 2 kudos

Validation on target stuck?

Hi All,I had 2 questions in my current journey learning stm32 software as well as my stm32f746g board. I generated code based off an .ioc file created by the AI Edge Dev Cloud (a human activity keras model). My issues are as follows: 1. I debugged th...

ramyg1_0-1738726555557.png ramyg1_1-1738726726916.png
ramyg1 by Associate
  • 880 Views
  • 1 replies
  • 0 kudos

Resolved! SD Card problem with sd-diskio.c generation

I have a simple program using Touchgfx and Freertos running on the following:STM32H735G-DKSTM32CubeIDE V 1.19.0STM32Cube_FW_H7_V1.12.1I have enabled SDMMC1 (in 1 bit mode, but 4 bit is the same), configured FATFS, and created a task to mount the SD c...

CYBR by Associate II
  • 1439 Views
  • 1 replies
  • 3 kudos

Resolved! adding code to a project without CubeMX deleting it

I have a project that is using AzRTOS, ThreadX, NetX, FileX, UsbX, and i'm still using cubeMX to reconfigure the hardware and drivers.  I understand that users need to put code between the "USER CODE BEGIN" and "USER CODE END" comments, if you're sti...

matt-crc by Senior III
  • 3142 Views
  • 3 replies
  • 1 kudos