STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1538 Views
  • 0 replies
  • 2 kudos

Resolved! CUBEMX 6.15 with Keil Full Assert bug

Same problem here (Cube 6.15.0, Keil uVision  Although HAL is selected, Cube installed both HAL and LL files for ADC and some other peripherals by mistake.  which results in a compile error ../Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_ll_adc.c(25...

regjoe_2-1758639075547.png regjoe_0-1758638667389.png regjoe_1-1758639027356.png
regjoe by Senior II
  • 1007 Views
  • 8 replies
  • 1 kudos

Error in STM32U5 MDF code generation

For a project based on the STM32U585 I use the MDF in a specific configuration.Filter 0: receives input from SIT0Filter 1 receives input from SIT3Filter 3 receives input from SIT0So three filters are used and only two serial input streams. Serial inp...

Leon3_0-1759241815651.png
Leon3 by Associate II
  • 626 Views
  • 3 replies
  • 1 kudos

Resolved! NUCLEO-H7S3L8 Debugging Code Running from XSPI NOR Flash

I created a Boot/App/ExtMemLoader project for my NUCLEO-H7S3L8 via the STM32CubeMX for STM32CubeIDE, and ran into issues when running the application code from the external NOR Flash chip on the NUCLEO board (U18, P/N MX25UW25645GXDI00 on the schemat...

rbtmkr42_0-1759118569172.png
rbtmkr42 by Associate III
  • 1046 Views
  • 4 replies
  • 1 kudos

Motor Control Timer Configuration PWM_PERIOD_CYCLES

We are migrating to a custom board and controller. Looking at the IOC generated by the Motor Control Workbench, there are some mystery variables that show up in the timer and we cannot track down where they are defined. See the attached snapshot and ...

gadams by Associate II
  • 443 Views
  • 1 replies
  • 0 kudos