STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1584 Views
  • 0 replies
  • 2 kudos

Anyone got STM32H7XX + I2S full-duplex master working?

I have tried to use STM32CubeMX and STM32CubeIDE to generate code. But in CubeIDE I can't create a SPI2_RX DMA Request. And in CubeMX I can't generate a Master Clock Output.So I wonder if there is any handcrafted code anyone written to get this worki...

DViks.1 by Associate II
  • 3039 Views
  • 6 replies
  • 0 kudos

STM32CubeMX 5.6.0 released

What is new in STM32CubeMX V5.6.0? • Added the support of new part numbers in the STM32L0 Series: STM32L071C(B-Z)Ux, STM32L081CZUx, STM32L072C(B-Z)Ux, STM32L082CZUx, STM32L073C(B-Z)Ux, STM32L083CZUx, and STM32L073CZUx • Added the support of the new 8...

FSMC with NAND interface signalling

Hello, I am using STM32L4R9AI (attached the reference manual) with 128GB NAND flash (MT29F128G08CFABBWP-12IT:B TR) (attached its datasheet).1- This is 8bit NAND flash and according to page 104 in the reference manual the last signal is NWAIT/INT whic...

Bug Report on Code Generation for NUCLEO-G474RE

Not a big bug but I wanted to mention it as it tripped me up.I am using STM32CubeMX 5.6.1 with IDE System Workbench 2.9.1I have found that when I setup SPI DMA synchronization the request number doesn't change from 1 when I generate the code or save,...

CH1 by Associate II
  • 2286 Views
  • 4 replies
  • 0 kudos

DMAContinuousRequests option does not appear on STM32Cube when setting up ADC with DMA. Therefore I can't make ADC work with DMA.

I am using the NUCLEO-H743ZI board. And I'm using STM32CubeIDE Version: 1.3.1Build: 6291_20200406_0752 (UTC) It has 3 16-bit ADCs, none of the three seem to have DMAContinuousRequests in the ADC settings:The DMA Settings tab is populated as follows:I...

0693W000001cIOfQAM.png 0693W000001cIPJQA2.png
FG by Associate
  • 1864 Views
  • 1 replies
  • 1 kudos

[Bug] Heap and Stack size of 0x00

The Linker Script is not being updated, if a heap or stack size of 0x00 is being written in MX and a code is being generated. Also mx.scratch won't be deleted.I'm using STM32CubeIDE v 1.3.1 and tried it on the L011F4 and L452RE controllers.To set the...

AScha.381 by Associate II
  • 1605 Views
  • 2 replies
  • 0 kudos