MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am using an ISM330DHCX device. I want to know how I can program the device to read the 12 registers, OUTX_L_G thru OUTZ_H_A in a continuous mode.

I know that CTRL3_C, IF_INC defaults to auto-increment of register address.I am trying to stream accel/gyro register data from the device by sending a SPI read command to register OUTX_L_G. The SPI controller is configured to read 12-bytes. The regis...

DBash.1 by Associate
  • 1288 Views
  • 1 replies
  • 0 kudos

LIS2DW12 Getting Falling Interrupt with Status register value 0 ?

Hello Support Team,I am working on the LIS2DW12 Sensor with Wake-up feature.Issue :Getting Zero on ALL_INT_SRC (3Bh) read while Falling interrupt occurred.Description :Configuration : Operation :Why does Falling Edge interrupt show Interrupt status a...

0693W00000Stl7GQAR.png 0693W00000Stl9bQAB.png
ChintaN1 by Associate III
  • 695 Views
  • 0 replies
  • 0 kudos

Multiple ROI procedure on VL53L1X using ULD - how to?

Hi,I'm using ULD to get measurements from VL53L1X. My case need to get 9 ROI - divided FoV into 3x3. When I run such measurement procedure it with 2x2 = 4 RoI - It's okay. But when I get 3x3 RoI in a similar way I get measurements such as max u16_t =...

MJ.2 by Associate
  • 1593 Views
  • 1 replies
  • 0 kudos

LSM6DSO32 FIFO Compression and FSM's

We are using the FIFO compression feature of the LSM6DSO32 which is working well for us if we use it standalone at 833 Hz. When we add the 4 FSM's that handle our motion recognition we start seeing duplicate tags in the compressed output implying tha...

Bobby123 by Associate II
  • 2019 Views
  • 3 replies
  • 0 kudos

Where can I find Linux drivers/example code for the LSM6DS33?

I have been looking for Linux drivers for the LSM6DS33 "iNEMO inertial module:always-on 3D accelerometer and 3D gyroscope", but have not had any luck. If anyone knows about any such repos or even references, it would be greatly appreciated.Thanks!

ST510 by Associate
  • 1166 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-BCN002V1B�?�ピアゾ素�?圧力センサーを�?��?��?��?�値を�?�り�?��?��?��?��?��?��?�??応�?��?��?�ん。

サンプルアプリをIAR�?�カスタマイズ�?��?�使�?��?��?��?��?�。アプリ�?�android�?�サンプルアプリを使�?��?��?��?��?�。注�?点�?��?�を教�?��?��??�?��?��?�。

ROnod.1 by Associate
  • 1601 Views
  • 3 replies
  • 1 kudos

Resolved! Algoritm reading FIFO LIS3DH

In my project, I used the LIS3DH chip. Most of the time the processor sleeps.The processor wakes up on time and on exceeding the shock threshold.In case of awakening on shock threshold, I need to read the data from the FIFO buffer (32 measurements) t...

MegaVolt by Associate
  • 1420 Views
  • 2 replies
  • 0 kudos