2022-03-08 1:49 AM
I'm trying to get data from PDM microphone and convert it to PCM data. This is my first project on stm32 and I'm starting to debug the project. Could you take a quick look at my code and say if you notice something wrong ? Some part of the code come from other project that have been shared here.
#include "main.h"
#include "pdm2pcm_glo.h"
#include "stdio.h"
/* Private variables ---------------------------------------------------------*/
SAI_HandleTypeDef hsai_BlockA1;
DMA_HandleTypeDef hdma_sai1_a;
UART_HandleTypeDef huart1;
PCD_HandleTypeDef hpcd_USB_FS;
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void PeriphCommonClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_DMA_Init(void);
static void MX_USB_PCD_Init(void);
static void MX_SAI1_Init(void);
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint8_t rxstate = 0;
/* PDM-PCM conversion configuration */
PDM_Filter_Handler_t PDM_FilterHandler;
PDM_Filter_Config_t PDM_FilterConfig;
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Configure the peripherals common clocks */
PeriphCommonClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
MX_USB_PCD_Init();
MX_DMA_Init();
MX_SAI1_Init();
PDM_FilterHandler.bit_order = PDM_FILTER_BIT_ORDER_LSB;
PDM_FilterHandler.endianness = PDM_FILTER_ENDIANNESS_BE;
PDM_FilterHandler.high_pass_tap = 2122358088;
PDM_FilterHandler.out_ptr_channels = 1;
PDM_FilterHandler.in_ptr_channels = 1;
PDM_FilterConfig.output_samples_number = 64;
PDM_FilterConfig.mic_gain = 1;
PDM_FilterConfig.decimation_factor = PDM_FILTER_DEC_FACTOR_64;
PDM_Filter_Init((PDM_Filter_Handler_t *)(&PDM_FilterHandler));
PDM_Filter_setConfig((PDM_Filter_Handler_t *)&PDM_FilterHandler, &PDM_FilterConfig);
uint16_t PDM_Buffer[128];
uint16_t pcm_data[4096];
uint16_t mid_Buffer[64];
//pcm_index = 0;
uint8_t pcm_index = 0;
HAL_SAI_DMAResume(&hsai_BlockA1);
HAL_SAI_Receive_DMA(&hsai_BlockA1, PDM_Buffer, 64);
while (1)
{
if (rxstate==1){
PDM_Filter(&PDM_Buffer[0], &mid_Buffer[0], &PDM_FilterHandler);
for(uint8_t i = 0; i < 64 ; i++){
pcm_data[pcm_index] = mid_Buffer[i];
pcm_index++;
}
rxstate=0;
}
if (rxstate==2){
PDM_Filter(&PDM_Buffer[64], &mid_Buffer[0], &PDM_FilterHandler);
for(uint8_t i = 0; i < 64 ; i++){
pcm_data[pcm_index] = mid_Buffer[i];
pcm_index++;
}
rxstate=0;
}
if(pcm_index==4096){
HAL_SAI_DMAPause(&hsai_BlockA1);
pcm_index = 0;
}
}
}
void HAL_SAI_RxHalfCpltCallback(SAI_HandleTypeDef *hsai_BlockA1){
rxstate = 1;
}
void HAL_SAI_RxCpltCallback(SAI_HandleTypeDef *hsai_BlockA1){
rxstate = 2;
}Update : Some parts of the code work not like I was expecting. About PDM_Buffer, only PDM_Buffer[0] gets a moving value : most of the time 0, sometime 7, sometime 64. All the other cases are stuck to 0. I don't know why this is happening.
Solved! Go to Solution.
2022-03-10 2:24 AM
Yes you can close the current topic as well. For the code, I took one from this link https://github.com/YetAnotherElectronicsChannel/STM32_PDM_Microphone/blob/master/code/Src/main.c#L200 and modified so it works as I intended.
2022-03-08 5:01 AM
I'm testing this code and so far, I can't get the PDM data into PDM_Buffer.
2022-03-10 2:13 AM
Hi @EEnco.1 ,
Can we close also the current topic, referring to this other thread?
Could you share here on the Community the solution you found to this issue?
-Eleon
2022-03-10 2:24 AM
Yes you can close the current topic as well. For the code, I took one from this link https://github.com/YetAnotherElectronicsChannel/STM32_PDM_Microphone/blob/master/code/Src/main.c#L200 and modified so it works as I intended.