MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS0X STEP COUNT READ BUG

After loading a new decission tree for the Machine Learning Core the behaviour of the Step count registers of the pedometer changed.I must note that none of the code changed, just the register mapping corresponding the decision tree loaded to the MLC...

PPill.1 by Associate
  • 1153 Views
  • 1 replies
  • 0 kudos

LSM6DSO32 taking High Current

I have powered from LSM6DSO32 through a 3V Coin cell battery and connected with Nrf52810 using I2C.Without any coding sensor taking around 2mA and after flashing its taking 4MA.I am getting the readings correctly.Attached the schematics

0693W00000SttviQAB.png
V.Jose by Associate II
  • 1857 Views
  • 3 replies
  • 0 kudos

Step count is non-zero even though object is stationary (LIS2DS12)

Hello ST,I am using LIS2DS12 sensor for step detection application. I read the step count register every 1 minute and reset the count value. I observe that even if the object is stationary, the step count register has a non-zero value (The value vari...

AB.4 by Associate II
  • 2401 Views
  • 5 replies
  • 0 kudos

LSM6DSxx Gyro "Ringing"

I'm trying to use several different IMUs in the LSM6DS family (LSM6DSOX and LSM6DSO32). Both of them are exhibiting "ringing" on the three gyro axes when exposed to shock (knocking the PCB against a table). It almost looks like there's no anti-aliasi...

JimJ by Associate
  • 1696 Views
  • 1 replies
  • 0 kudos

the sensory library does not work at all.

Hello, I'm working on a project involving voice recognition. So, I used the stm32 sensory library to complete this project and the MP23DB02MM digital MEMS PDM microphone. However, I only found one example that used STM32H747I-DISCO, so I ported it to...

0693W00000SuITyQAN.png 0693W00000SuIToQAN.png 0693W00000SuIXCQA3.png

Read lsm6dso32 data via libiio

We are trying to use lsm6dso32 accelerometer/gyroscope connected to a custom hardware (non-st) via i2c. What we want to achieve is reading measured values continuously, ideally via libiio (buffered).We are building a custom linux (kernel version 5.4)...

NKuhn.1 by Associate II
  • 2557 Views
  • 3 replies
  • 0 kudos

Resolved! TDM interface with SAI for LIS25BA

Hi,I try to use a custom board with LIS25BA.I use SAI with STMF446.What I know :MCLK = 12.288 MHzWCLK = 16kHz8 slot with 3 activeso BCLK = WCLK * (8 * 16) = 2.048 MHzWhat I can do :I2C works like a charm ;)What I can't do :Configure SAI with these va...

0693W00000Stzc9QAB.png 0693W00000StzedQAB.png
Axoul by Associate
  • 1768 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.