MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Multiple ROI procedure on VL53L1X using ULD - how to?

Hi,I'm using ULD to get measurements from VL53L1X. My case need to get 9 ROI - divided FoV into 3x3. When I run such measurement procedure it with 2x2 = 4 RoI - It's okay. But when I get 3x3 RoI in a similar way I get measurements such as max u16_t =...

MJ.2 by Associate
  • 1625 Views
  • 1 replies
  • 0 kudos

LSM6DSO32 FIFO Compression and FSM's

We are using the FIFO compression feature of the LSM6DSO32 which is working well for us if we use it standalone at 833 Hz. When we add the 4 FSM's that handle our motion recognition we start seeing duplicate tags in the compressed output implying tha...

Bobby123 by Associate II
  • 2089 Views
  • 3 replies
  • 0 kudos

Where can I find Linux drivers/example code for the LSM6DS33?

I have been looking for Linux drivers for the LSM6DS33 "iNEMO inertial module:always-on 3D accelerometer and 3D gyroscope", but have not had any luck. If anyone knows about any such repos or even references, it would be greatly appreciated.Thanks!

ST510 by Associate
  • 1218 Views
  • 1 replies
  • 0 kudos

Resolved! STEVAL-BCN002V1B�?�ピアゾ素�?圧力センサーを�?��?��?��?�値を�?�り�?��?��?��?��?��?��?�??応�?��?��?�ん。

サンプルアプリをIAR�?�カスタマイズ�?��?�使�?��?��?��?��?�。アプリ�?�android�?�サンプルアプリを使�?��?��?��?��?�。注�?点�?��?�を教�?��?��??�?��?��?�。

ROnod.1 by Associate
  • 1675 Views
  • 3 replies
  • 1 kudos

Resolved! Algoritm reading FIFO LIS3DH

In my project, I used the LIS3DH chip. Most of the time the processor sleeps.The processor wakes up on time and on exceeding the shock threshold.In case of awakening on shock threshold, I need to read the data from the FIFO buffer (32 measurements) t...

MegaVolt by Associate
  • 1479 Views
  • 2 replies
  • 0 kudos

LIS2DTW12 FIFO threshold interrupt not correct

Hello,I'm using a LIS2DTW12, here the configuration :ODR 400HzFIFO threshold on INT2 push pull interrupt. Threshold 16Continuous mode All seems to work correctly but sometimes I have an incorrect interrupt. The INT2 signal is yellow, the purple is a ...

0693W00000QOIkOQAX.png 0693W00000QOIlqQAH.png 0693W00000QOImAQAX.png
RStra by Associate III
  • 907 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.