MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Lis2dh12 behaviour of i2c peripheral while powered off

Hi.I'm currently working on an application where I have a lis2dh12 accelerometer sharing an i2c bus with another sensor. These sensors need to be turned off by cutting off the power on the Vdd line. I'm running into issues with communicating with the...

Jonki by Associate
  • 1339 Views
  • 0 replies
  • 0 kudos

Resolved! What are the transfer functions of LPF1 and LPF2 for LSM6DSOX?

I am interested in calibrating precisely the delay introduced by the filter chain (LPF1 and/or LPF2) of the LSMDSOX (or DSO/DSM - I presume they are the same). I have found the settling times in Table 13 of App Note AN-5272, which is a good start, bu...

lgi000 by Associate
  • 2124 Views
  • 2 replies
  • 0 kudos

I am using IIS3DWB accelerometer for condition monitoring. In order to offset DC I intend to use HP filter ODR/800 which gives me high pass cutoff 33Hz. I wonder how to capture frequencies for a range below 33.3Hz (equipment running at 1500rpm (25Hz)?

I intend to use IIS3DWB accelerometer for machine vibration monitoring. In order to offset DC I intend to use HP filter ODR/800 which gives me high pass cutoff 33Hz. I wonder how to capture frequencies for a range below 33.3Hz (equipment running at 1...

AGosw.3 by Associate
  • 1298 Views
  • 1 replies
  • 0 kudos

MKSBOX1V1 and SPBTLE-1S module

Hopefully someone can assist:I am using the ST EVAL-MKSBOX1V1 (aka Sensortile Box) and trying to set up the SPBTLE-1S for use with STM32duino. I tried to follow the instructions in the STM32duino pages (here: https://github.com/stm32duino/Arduino_Cor...

GEmel.1 by Associate II
  • 3416 Views
  • 5 replies
  • 0 kudos

Resolved! IIS328 how to get out of an I2C hang

I'm using a IIS328DQ on an I2C bus @400KHzEvery now and again, the part hangs up and won't talk to me.  The only way out that I've found is a power reset.Attempting to follow https://community.st.com/t5/mems-sensors/if-hang-up-i2c-interface-of-the-li...

RLee4_0-1687460642025.png
RLee.4 by Associate III
  • 3860 Views
  • 5 replies
  • 0 kudos

LSM6DS3 Data Ready Interrupt not triggering

Hi everyone,I am working on a project using the SensiBLE module. It includes an STM32L476RG microcontroller and an LSM6DS3 IMU sensor. I am using I2C for communication between the two.I am trying to enable the accelerometer data-ready interrupt on IN...

MEMS Microphones frequency response until 20 kHz

Hello,I contact you because I am considering three models of MEMS microphones for an application: MP34DT05-A, IMP34DT05 and MP34DT06J.Inside the datasheet the frequency response is depicted until 10 kHz.Are these microphones suitable for an applicati...

VROM by Associate
  • 4004 Views
  • 5 replies
  • 0 kudos

Resolved! ISM330DLC measurement units

What are the units of the ISM330DLC reported values? SpecificallyOUTn_G to units of acceleration (g)?OUTn_XL to units of angular velocity (°/s)?I couldn't find this in your docs, may have missed it