cancel
Showing results for 
Search instead for 
Did you mean: 

Thermal response

Macneacail
Associate III

One of the critical measurements for the analysis of bridges is the thermal response. The 201/109 combination has an average thermal response in the FFT of 1.5 milli-g - it is slightly frequency dependent, but ignoring that the standard deviation means that below 3.5 milli-g is just Gaussian data. Anything over 3.5 is structural response, statistically speaking. The 3.5 milli-g is higher than other accelerometers we use, do you have some device with a tighter response to thermal?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Federica Bossi
ST Employee

Ciao @Macneacail​,

For your application, I suggest you to look at IIS2ICLX and let me know if you need more information.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Macneacail
Associate III

It is 2 axis only, of no use in bridges, but we are testing the 201/109 in 12 locations, so we will know a lot more in 12 months.