MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! i am using lsm6dsm (@steval-mki189v evaluation board) for OIS application, data sheets says, auxiliary spi can be used for the purpose, also through the primary spi we can read the data parallely, like connecting host processor and camera module in mode 3

but i am not able to read the data in slave module, how to connect this with the host and camera module processor and read the data, is there any settings have to be mentioned.? if any one information about this it will be helpful.

BGGopal by Associate II
  • 4036 Views
  • 7 replies
  • 0 kudos

Resolved! how to convert LSM6DSOX data

Hi all,I'm working with LSM6DSOX and I managed to get the accelerometer and gyroscope data from the output registers, but the numbers don't seem to be meaningful, how do I convert the raw data to g?

Is accelerometer drift in the LIS3DSH normal behavior?

I have an LIS3DSH securely mounted to a stationary object away from any vibration. Over the course of two and a half days, I've found the readings slowly change in value. I've tried this with multiple accelerometers (all LIS3DSH) and they always sh...

0690X00000ArfS2QAJ.png 0690X00000ArfS7QAJ.png 0690X00000ArfSCQAZ.png

Resolved! Re: X-nucleo-iks01a3's SPIs?

1. Are SPI_MISO/MOSI/CK/CS connected to STM32 MCU on the board? Logic Level 1.8V?2. Are SPI_MISO/MOSI/CK/CS_O for external connections on the board? Logic Level Vio?3. Are there a dedicated shunt for Vio connecting to 3.3V on the board?4.If a 3.3V lo...

QShan.1 by Associate II
  • 1453 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSV - gyroscope bias

Hello ST community. I'm currently working with a LSM6DSV in a drone application. I would like to known if there is a suggested way to cancel the gyroscope bias value?

Resolved! ST BLE SENSOR APP MICROPHONE

Hello could someone explain me for the FFT LINE COMPARE that is in the ST BLE SENSOR APP for the sensortile.box what are the parameters that appear to edit? and also for the FFT COMPARE, which I understand that it will be the same and the "Name file ...

SAbba.1 by Associate III
  • 3710 Views
  • 2 replies
  • 0 kudos

Query about LSM6DSR read/write address on I2c interface

I am using LSM6DSR on I2c interface. As per datasheet when the SDO/SAO pin of the sensor is connected to ground the read/write address should be D5H/D4H but currently the read/write address is D7H/D6H. Can you please explain the reason for this? Has ...

RWasw.1 by Associate II
  • 4047 Views
  • 5 replies
  • 0 kudos