cancel
Showing results for 
Search instead for 
Did you mean: 

ILPS22QS Cleaning After Soldering

DBass.2
Associate

TN0018 calls out in the Process considerations section that the board must be properly cleaned after soldering if "self-cleaning" solder paste is not used. Are there any guidelines on cleaning methods that will not damage the sensor? Can the sensor port be covered with something like Kapton tape to protect it during the cleaning process?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @DB.7assett​ ,

Welcome to ST Community!

There are too many cleaning procedure that are dependent to manufacturer (and sometimes also to the used oven). For pressure sensor devices there are two methodology to use to avoid to damage the device:

1. don't use the Kapton over the window of device because the glue can close the small holes. 

2. It is mandatory don't use vapor phase machine for soldering.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @DB.7assett​ ,

Welcome to ST Community!

There are too many cleaning procedure that are dependent to manufacturer (and sometimes also to the used oven). For pressure sensor devices there are two methodology to use to avoid to damage the device:

1. don't use the Kapton over the window of device because the glue can close the small holes. 

2. It is mandatory don't use vapor phase machine for soldering.

If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster!

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.