MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issues with LIS2DW12 temperature sensor in Single data mode

Hello, guys!Could you help us understand the issue with single data conversion for an internal temperature sensor of LIS2DW12? While experimenting we followed datasheet (DS11811 - Rev 8), Application Note AN5038 and single data conversion app note DT...

stKAT by Associate
  • 1666 Views
  • 1 replies
  • 1 kudos

STEVAL-MKI185V1 integration with LabView

Hi,I have STEVAL-MKI185V1 adaptor. ST Microelectronics is already giving the software. But I would like to integrate the output from the motherboard through LabView. Can someone please tell me whether it is possible to use LabView as acquisition soft...

Jongyul by Associate
  • 1816 Views
  • 2 replies
  • 0 kudos

ASM330 SPI robustness

We are planning to use ASM330LHH at a distance of about 1m from the MCU to which it will interface for supplying the gyro data in an automotive application. SPI will run at around 1MHz. Can we interface directly through SPI, or should we integrate th...

VikasP by Associate
  • 3252 Views
  • 4 replies
  • 0 kudos

Resolved! X-CUBE-GNSS1 software package and the X-NUCLEO-IKS01A2

puis-je utiliser le progiciel X-CUBE-GNSS1 et la carte d'extension X-NUCLEO-IKS01A2 avec une carte Nucleo STM32 pour développer une application combinant à la fois les fonctionnalités GNSS et les capteurs MEMS ? Si oui, comment puis-je les connecter ...

khairi by Associate II
  • 2557 Views
  • 3 replies
  • 0 kudos

Resolved! IIS3DWB sensitivity and resolution

I would like to find out the if the following assumptions are correct. It offers 16 bit (65K) level resolution. The sensitivity in mV/g would about 3000/2g for the 2g range? That seems rather high because typically you see 500 mv/g values. Also I am ...

Sudhir by Associate III
  • 3429 Views
  • 4 replies
  • 0 kudos

STWINBX1 and HSDATALOG = Corrupt Data when converting to CSV

I am running a STWINBX1 with the latest v1.2.0 firm from the STM32CubeFunctionPack_DATALOG2_V1.2.0.I have compiled and uploaded the DATALOG2-STWIN.Box firmware successfully.  I am using the ST BLE Sensor App v5.0.0 on my iPhone to configure and run t...

WP by Associate III
  • 6603 Views
  • 14 replies
  • 0 kudos

UNICO GUI ODR

Hello,There are some abbreviations next to ODR: HP, HA, LP1, LP2, LP3, and NM. I believe HP stands for high performance, LP stands for low performance, and NM stands for normal mode. Can you explain the differences between LP1, LP2, and LP3? Addition...

FKara.3 by Senior
  • 1743 Views
  • 1 replies
  • 0 kudos

LSM6DSO(X) SPI communication problems

Hello!I have a working version of the chips with the marking on the surface "S4 052"Recently we've received a new batch of LSM6DSO(X) chips - they don't respons to ID requests via SPI. The marking on the surface of the new chips is "S4 148".What the ...

Mappy by Associate
  • 1818 Views
  • 4 replies
  • 0 kudos