User Activity

Hi All!I'm doing a project on the STM32F429 discovery board.In this project, I've used the TouchGFX.Also, I'm using the FreeRTOS. The idea is to read the Temperature sensors and read their values to the TextAreas in TouchGFX.TouchGFX was tested and w...
Hi all!I have a problem with transmition/receiving more than 8 bytes of data between two STM32 MCUs via CAN-Network.I know, it is impossible to transmit more than 8 bytes of data via basic CAN Bus.I tried to create Command messages System.CAN Master ...
Hi,I designed and tried to use my custom board based on STM32F030R8T6 MCU. But the problem started from beginning.For MCU Flashing I used STM32CubeProgrammer and ST-LINK V2 (STM8 & STM32) dongle. First of all I was trying to connect the board and I'v...
Hello Everyone!I've tried to configure SD Card to STM32F030R8T6 via SPI1.For reference I took this link: https://controllerstech.com/sd-card-using-spi-in-stm32/After configuration CubeMX in STM32CubeIDE I've got the start code.Without any other codin...
Hello Everyone!Couple days ago, I tried to interface STM32F030R8T6 dev. board with TFT display like on the picture with ILI9486 driver.One year ago, I interfaced the same TFT with FPGA de board and everything was fine.With STM32 I tried to interface ...
Kudos from
Kudos given to