cancel
Showing results for 
Search instead for 
Did you mean: 

What is the purpose of VDDIO in ISM330DLC Accelerometer

NSemrHomeInit
Senior

Dear ST,

I am using the ISM330DLC gyro and accelerometer,

In the electrical connection mode 1 I have a pin called VDDIO.

In my application I connected this pin to 3V but, I don't have any idea what is the use of this pin?

Thank you for explaining

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Well, that's in the data sheet, table 1, with the pin descriptions:

VDDIO(1) Power supply for I/O pins

Footnote 1 stands for: Recommended 100 nF filter capacitor.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Well, that's in the data sheet, table 1, with the pin descriptions:

VDDIO(1) Power supply for I/O pins

Footnote 1 stands for: Recommended 100 nF filter capacitor.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
NSemrHomeInit
Senior

Hello Peter,

I think that means If I want 4.5v on INT1/2, went the interrupt is triggered, I have to connect VIO to 4.5v?

The data sheet clearly states in Table 3:

Vdd_IO = Power supply for I/O, min 1.62V, max 3.6 V

4.5V are slightly above 3.6V, so they are not permitted.

If you need a different voltage level because the connected components work there, you still have to keep within the voltage range for VDDIO and use a level shifter at INT1 or INT2, for example.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.