STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1563 Views
  • 0 replies
  • 2 kudos

STM32CubeMX, FreeRTOS and Signals

Posted on September 10, 2014 at 16:50I use CubeMX to add FreeRTOS to my project, currently running on a 429 discovery board. Cube adds FreeRTOS and a CMSIS-RTOS wrapper.I'd like the use the FreeRTOS Event Groups or the CMSIS-RTOS Signals but Event G...

rreay by Associate II
  • 2270 Views
  • 4 replies
  • 0 kudos

STM32CubeMX configuration bug report

Posted on March 18, 2015 at 07:28I use the STM32CubeMX. However, it has a wrong configuration problem for UART. I want to use the asynchronous RX only mode, but it's not configurable. My configuration procesures: 1. Configuration -> Peripherals -> U...

just4you by Associate III
  • 1036 Views
  • 1 replies
  • 0 kudos

Clock settings in CubeMX 4.6 doesn't work for F072

Posted on March 22, 2015 at 10:45 I am using CubeMX 4.6.0 with STM32Cube FW 1.2.1 for a STM32F072 chip. I am having trouble getting the clock settings code to work properly. I have activated some ADC features in CubeMX, which turns o...

jesper by Associate II
  • 1606 Views
  • 2 replies
  • 0 kudos

STM32F4 Discovery + CUBEMX + Ethernet (dp83848)

Posted on March 23, 2015 at 15:59NOTE: edited by moderator on Oct 6th, 2016 Hello, I have working example project for STM32F4 Discovery with dp83848 phy, from [[this link/image has been flagged as malicious by our security scan software and has b...

maku0 by Associate
  • 2246 Views
  • 1 replies
  • 0 kudos

STMCube/HAL for STM32F4 - Suggestions

Posted on March 17, 2015 at 14:24Hello everyone,I am about to start a commercial product with STM32F429 MCU and have previous knowledge with std_periph_drivers. Since I have already read about bugs with HAL drivers sometimes before, would you sugges...

predrag10 by Associate II
  • 1053 Views
  • 1 replies
  • 0 kudos

STMCubeMX STM32F411RE MX_DMA_Init()

Posted on March 10, 2015 at 01:47I have created an STMCubeMX project for the STM32F411RE Nucleo board and it is going pretty well until I tried to use DMA.  I do not get very far because in no case does the MX_DMA_Init() function get created.  The f...

Does CubeMX code generator has some problems in I2C or not?

Posted on February 19, 2015 at 10:31I'm a beginner in stm32Fx. I'm using Keil IDE and cubeMX code generator.I've used I2C1 and I2C3 in my board with stm32f407 microcontroller and used cubeMX for generating initial codes. I've tried to use I2C3 and i...

hamid by Associate
  • 5272 Views
  • 11 replies
  • 0 kudos

CubeMX pin configuration issue with STM32L152QEHx UFBGA132

Posted on February 23, 2015 at 22:49In attempting to validate a schematic design in progress I used CubeMX to verify that none of the I/O assignments and peripheral functions being called out in the schematic were going to conflict.  I noticed that ...

seth by Associate II
  • 1438 Views
  • 2 replies
  • 0 kudos

STM32cubeMX in MATLAB Support.

Posted on February 19, 2015 at 05:25I , just installed the updated version of STM32 MAT target 4.0 version in my matlab 2014a . now there is one  block regarding MCU Configuration in which , I have to provide one .ioc file for configuration . My que...

13meep34 by Associate II
  • 1531 Views
  • 2 replies
  • 0 kudos