STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1567 Views
  • 0 replies
  • 2 kudos

Possible bug in STCubeMX HAL DMA code for F4

Posted on August 13, 2014 at 02:14I do not know enough about the internal workings of the processor to be sure, but I believe there is a bug in the HAL DMA drivers for the F4xx series. Specifically, it seems the De-init method puts the DMA periphera...

jwoolston by Associate II
  • 1555 Views
  • 3 replies
  • 0 kudos

Stm32Cube - Simulink - MikroC

Posted on October 01, 2015 at 13:22Hello, I'm new here and i've the problem that i don't know how to get the generated code from simulink and CubeMX to my Microcontroller.My Setup:I use mikroC Pro and an EasyMX Prov7 board with STM32V107VCT6Now I go...

Problem with USB Host CDC class

Posted on July 03, 2014 at 12:01Hello,I'm using STM32CubeMX to generate a project for STM32F207 that uses USB Host. The project compiles without problems. I have a custom USB device that uses CDC to send and receive serial data. When the device is a...

BUG: CAN race condition if HAL_CAN_Receive_IT is used

Posted on April 15, 2015 at 22:27 If you use HAL_CAN_Receive_IT for receive and send messages at same time you can get race condition. Typical callback looks like: void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef* CanHandle) { if ((CanHandle...

vromanov by Associate II
  • 3846 Views
  • 6 replies
  • 0 kudos

Request STM32cubeMX to work with latest Java

Posted on July 23, 2015 at 09:41Due to security reasons I recently updated to the latest Java 8 Update 51 (Releasedate 14.07.2015) and deleted the old Java version. But now CubeMX (4.9.0) is not starting anymore asking for an old Java 1.7.0_45 I kin...

ramm by Associate II
  • 1279 Views
  • 5 replies
  • 0 kudos

STM32F103 HAL UART: TX error, HAL_BUSY (FreeRTOS)

Posted on September 12, 2015 at 00:46Hi All,I'm trying to build an application which can receive commands through UART, and can also send messages.I have created 2 threads using FreeRTOS: one for a continuous RX, and one for a repetitive TX.The RX t...

balazs by Associate II
  • 1279 Views
  • 1 replies
  • 0 kudos

need very simple UART RXNE and IDLE interrupt example

Posted on September 08, 2015 at 12:25 Hello, I've used the STD peripheral libraries before and successfully generating interrupts from UART //snippet 1 void USART1_IRQHandler(void){ char chee; if(USART_GetITStatus(USART1, U...

krishna2 by Associate
  • 7644 Views
  • 3 replies
  • 0 kudos

STM32CubeMX and HAL Libraries Version (F1 for my case)

Posted on September 02, 2015 at 04:35Hello,I just start using STM32CubeMX three days ago and the product is looking good! I'm playing with a Nucleo Board STM32F103RB and one thing that I noticed is that the HAL Library for F1 version downloaded by C...

kopf by Associate II
  • 1939 Views
  • 2 replies
  • 0 kudos

STM32CubeMx Adding own plugin.

Posted on July 24, 2015 at 14:41Hello, I am developing own RTOS for STM32. I see that CubeMX is a very useful tool for generating SW configuration. Is there any possibilty to add my OS to CubeMX configuration? I saw that configuration of IP packages...

slawek by Associate III
  • 717 Views
  • 1 replies
  • 0 kudos