cancel
Showing results for 
Search instead for 
Did you mean: 

Request STM32cubeMX to work with latest Java

ramm
Associate II
Posted on July 23, 2015 at 09:41

Due to security reasons I recently updated to the latest Java 8 Update 51 (Releasedate 14.07.2015) and deleted the old Java version.

But now CubeMX (4.9.0) is not starting anymore asking for an old Java 1.7.0_45

I kindly ask you to make the CubeMX software compatible to the latest Java.

And I also ask other users to support this request.

#java-jre #stm32cubemx #stmcube
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
ramm
Associate II
Posted on July 24, 2015 at 13:57

No comments and only very few views... does nobody care about using an obsolete Java with security issues?

Amel NASRI
ST Employee
Posted on July 24, 2015 at 16:01

Hi ramm.nils,

Your feedback is under review.

No comment on your post doesn't always mean ''no care'' :)

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on July 24, 2015 at 19:41

No comments and only very few views.

Says a guy with TWO total posts to the forum, with ONE of them bitching about the fact nobody commented on the other post... Participation is a two-way street.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
stm32cube-t
ST Employee
Posted on August 27, 2015 at 20:02

Dear user,

CubeMX 4.9 works fine using latest java 8 jre_8u60.

Best regards
ramm
Associate II
Posted on September 14, 2015 at 12:28

I confirm CubeMX 4.10 works fine using latest java 8 jre_8u60 64bit on Win7.

Thank you