STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1627 Views
  • 0 replies
  • 2 kudos

STM32CubeMX GCC Linker BUG for STM32L151RCTx

Posted on July 11, 2015 at 05:06Hi, been using STM32CubeMX for creating code for ''System Workbench for STM32''. The linker file created by STM32CubeMX has 0 for heap and stack: _Min_Heap_Size = 0;      /* required amount of heap  */ _Min_Stack_Size...

CubeMX - STM32L1 USB CDC

Posted on May 12, 2015 at 09:45Hello,I have set up a CubeMX project with USB FS and CDC enabled. The device is STM32L151CCT6.Also, I have installed the VCP 1.4.0 drivers for Win7 (x64).When I start the debug session (IAR 7.40), Windows complain that...

George.P by Associate III
  • 2489 Views
  • 5 replies
  • 0 kudos

Bug in STM32CubeMX clock configuration

Posted on November 12, 2015 at 13:52Experiment Set-up:STM32CubeMX version: 4.11.0STM32F746NGH6Description:It limits the PCLK1 to 50 MHz and PCLK2 to 100 MHz. See the RED error below:However, The PCLK1 can reach 54 MHz and PCLK2 can reach 108 MHz aft...

0690X00000602aZQAQ.jpg 0690X00000602aFQAQ.jpg
wenbin by Associate II
  • 1449 Views
  • 2 replies
  • 0 kudos

TIM3 problem in stm32 cube HAL library

Posted on November 30, 2015 at 09:52Hello.I am using STM32F0xx with stm32cube lib as the dev platform. My application requires TIM3 peripheral. I am using __HAL_TIM_SET_COUNTER to set the cnt value at runtime. I need the timer count value for some c...

CubeMx USB CDC asynchronous API?

Posted on May 24, 2015 at 18:38Hello All, 1) how can I have an asynchonous Transmit command ? 2) what is the largest amount of data I can put into CDC_Transmit_FS ? I am implementing CDC on my firmware based on CubeMx. So far it works (I have to inc...

taraben by Senior
  • 1987 Views
  • 3 replies
  • 0 kudos

STM32CubeMX sample

Posted on November 24, 2015 at 12:51Hi, It's not very useful have the sample code for STM32CubeMX without the STM32CubeMX  file!! Where are the *.ioc file!!!!! #stm32cubemx

CubeMX code generation problem

Posted on March 03, 2015 at 00:30Hi,I did a initialization  project with CubeMX for STM32F4discovery but when I click ''generate source code'' (selecting IDE MDK-ARM 4.73 and firmware package STM32Cube FW_F4 V1.4.0) appears the error message:''the c...

STM32F429 & STM32cubeMX

Posted on October 30, 2015 at 11:05Hello all, when I am using STMcubeMX I can not find the SPI6 peripheral, but according the datasheet STM32F429AIH7 has SPI1, SPI2, SPI3, SPI4, SPI5 and SPI6 . thanks in advance. #spi6-stm32cubemx-stm32f429

diego23 by Associate
  • 1299 Views
  • 2 replies
  • 0 kudos