STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1564 Views
  • 0 replies
  • 2 kudos

STM32F042: UART application using CubeMX not working

Anyone Helps me!Anyone please show the basic USART's tx/rx code. Or check my CubeMX Project File.HAL's USART won't work.it code is generate from STM32Cube.There is two USART, one(huart2) everytime send data to STM, another(huart1) everytime wait comm...

ssako by Associate II
  • 4665 Views
  • 9 replies
  • 0 kudos

Resolved! Hi, i am trying tu use nucleo extender <nucleo-IHM14A1> with <nucleo-F446RE> bord. But I'm facing problems.

As STM32CubeMX 4.25.1 is not compatible with <X-CUBE-SPN14> Stepper motor driver software expansion for STM32Cube package, i tried to include manualy the Driver to my project. Then, i copy the <BSP> repertory from <en.x-cube-spn14\...\Drivers> to my ...

Resolved! STM32F7 Problem triggering ADC3 with TIM6

Hi, I'm using STM32F746ZG Nucleo board, Atollic Truestudio and STM32CubeMX for generate source code. I'm trying for a couple of days to configure Update Event of TIM6 to trigger ADC3 .There isn't problem with TIM1 triggering ADC3 (Edit Line 104: hadc...

JFerr.8 by Associate
  • 1607 Views
  • 2 replies
  • 1 kudos

Generated code from CubeMX 5 does not compile on OpenSTM32

I have a problem with a new generated code from CubeMX 5 (latest version), when compiling it with the latest version of OpenStm32. I am using SPI, I2C, UART, ADC-IN10, RTC and ext. 32kHz QuarzHere are some of the errors I receive:Description Resource...

BerndE by Associate II
  • 1058 Views
  • 0 replies
  • 1 kudos

CubeMX 4.24 LL Drivers generation bugs

Posted on February 19, 2018 at 08:44Hi ,First of all,i want to thank ST for providing and developing such useful tools for developers.Found couple of bugs in STM32CubeMX v 4.24 U(S)ART code generation when using LL Drivers During my work ,I wrote an...

Michael N by Associate II
  • 2008 Views
  • 5 replies
  • 0 kudos

Resolved! problems with usb msc device on stm32f4

Hi. I need to create USB MSC Device on STM32F407. I use CubeMX for create project. When I compiled the project with MSC_MEDIA_PACKET = 512 windows did not see the mass storage device, then I changed MSC_MEDIA_PACKET = 256 and windows saw the mass sto...

MishaT by Associate II
  • 1776 Views
  • 1 replies
  • 0 kudos

Issues with CubeMX version 5.0.1

Hi, I have updated CubeMX to version 5.0.1 and after this I noted an issue in Micro Vision 5 which I have no idea how to resolve. I am new in STM32 world, just have a couple of months since started to learn.I use to put user labels on GPIOs, it is mu...

VIO47 by Associate II
  • 4914 Views
  • 9 replies
  • 0 kudos