MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STHS34PF80 Abnormal operation

When STHS34PF80 detects the human body for a period of time, TPRESENCE cannot fall back normally, and pres_flag is always 1。 code:

top_0-1711014368016.png
top by Associate
  • 1113 Views
  • 3 replies
  • 0 kudos

LPS22DF Temperature compensation

Hi,I want to compensate for the temperature of the LPS22DF sensor.how does one go about programming for it? Is this formula correct?Pcorrected​=Pmeasured​−(TCF×(Tmeasured​−Treference​))If it is, should I use a temperature reference value of 25°C?Also...

nu by Associate
  • 523 Views
  • 0 replies
  • 0 kudos

Resolved! magnetometer Calibration Library does not work

Hello,    I am working on a custom board based on STM32F407 CPU with the LSM6DSV16XTR accelerometer+gyroscope and LIS2MDLTR magnetometer.The aim is to get board inclination and compass information with the maximum accuracy.The MotionFX library seems ...

MRaff.1 by Associate III
  • 2357 Views
  • 3 replies
  • 0 kudos

Resolved! LPS22DF I3C addressing

Dear forum,We plan to assemble five LPS22DF sensors on the same I3C bus and (off course) to address them individually. According to the datasheet (7.4.1 MIPI I3CSM CCC supported commands) the answer to GETPID can only have two values, depending on SD...

tcachat by Associate II
  • 1041 Views
  • 1 replies
  • 0 kudos

LIS3MDL not responding over SPI on custom PCB

Hi,I'm designing a flight controller pcb using several ST mems sensors, (LSM6DSO, LIS3MDL, LPS22HH) and interfacing them to an STM32H743IIT6 microcontroller over a shared SPI bus. I'm on the second iteration of this board, all sensors worked on the f...

VictorK_7-1725716130081.bmp VictorK_8-1725716140311.bmp VictorK_6-1725714206425.png VictorK_2-1725713533727.png
VictorK by Associate
  • 1196 Views
  • 2 replies
  • 2 kudos