cancel
Showing results for 
Search instead for 
Did you mean: 

LPS22DF Temperature compensation

nu
Visitor

Hi,

I want to compensate for the temperature of the LPS22DF sensor.

how does one go about programming for it?

 

Is this formula correct?
Pcorrected​=Pmeasured​−(TCF×(Tmeasured​−Treference​))
If it is, should I use a temperature reference value of 25°C?
Also, can you tell me the value of the Temperature Compensation Factor?

 

Can I make a correction formula with TCO(Temperature coefficient offset) with a data sheet and program it?

If possible, please let me know the formula that I can use TCO

 

Thank you

0 REPLIES 0