User Activity

The ISM330IS product embeds a general-purpose core, a new ST category of processing, called ISPU (intelligent sensor processing unit). The ISPU is based on STRED architecture, a proprietary architecture developed by STMicroelectronics. Its optimized ...
Save the date --- APRIL 28, 2022, SEMI HQThis class will explain and demonstrate how AI/ML logic can be implemented on Edge devices such as Smart sensors. Power efficiency, latency, and bandwidth considerations are important for AI/ML implementation ...
This article describes how to configure the Machine Learning Core (MLC) on IIS2ICLX to implement the detection of the tilt angle, i.e. the current inclination of the device, in the range of -20 to +20 degrees. The hardware used is the ProfiMEMS with ...
This article deals with the implementation of a simple machine learning case (the recognition of the state of an asset in movement) on the LSM6DSOX core of the SensorTile.box, combined with a finite state machine configuration that determines the fre...
This article deals with the implementation of a simple machine learning case (the recognition of the state of a door) on the LSM6DSOX core of the SensorTile.box, and the visualization of the output of the decision tree on the STBLE Sensor smartphone ...
Kudos from
Kudos given to